TouchGFX: Generated Code Using Pins on Pins Used for Other Features
- 1 reply
- 1366 views
Hello,
I am using the STM32H7B3I-EVAL evaluation board to develop an understanding on using a custom board that has an LCD display. I am dissecting the code and there is something inconsistent that I am trying to understand.
My steps were as followed:
1) Use CubeMX to bring up the code from scratch, adding the TouchGFX 4.20.0 software package.
2) Open the ApplicationTemplate.touchgfx.part file to generate the code for the UI.
3) Made a basic display UI (one screen with a red background, just to test).
The code works without issue, but I am looking through the TouchGFX folder to understand the code and there is a file created:
TouchGFXGPIO.cpp ( I have attached it).
It's claiming it's using 4 signals (VSYNC_FREQ, RENDER_TIME, FRAME_RATE, MCU_ACTIVE), which toggles the following pins:
// VSYNC_FREQ - Pin PA4
// RENDER_TIME - Pin PG13
// FRAME_RATE - Pin PB15
// MCU_ACTIVE - Pin PG12
On the evaluation board, those pins are used for different features entirely.
PA4 - DCMI_PIXCLK or I2S6_EXT_SD
PG13 - LED1
PB15 - T_VCP_RX
PG12 - SDIO2_D3
Despite the connection to these pins, I am surprised the code still works. Can anyone explain the purpose of this file and why triggering these pins are necessary?