Skip to main content
Ofaro.1
Associate III
Feb 12, 2025 12:41 PM UTC
Question

TouchGFX Frame Buffer: image inverted at corners

Hi,

I'm facing an issue displaying an image on a 1024x600 screen via RGB. As shown in the image, the frame buffer is displaying part of the image as an inverted image in the corners. I've double-checked the LCD timing parameters, and they all match the datasheet specifications.

I'm using a custom board based on the STM32F429 with external SDRAM.

Please find the attached images for the current configurations.

Your suggestions will be highly appreciated.

Thanks

This topic has been closed for replies.