Skip to main content
Associate
Aug 5, 2025 12:36 PM UTC
Solved

TouchGFX font distorted

I have TouchGFX UI running on STM32H7. Only with one screen there is an issue, fonts gets distorted.

VNA_0-1754397210983.png   VNA_2-1754397269439.png

What could be the reason for this?

 

 

This topic has been closed for replies.
VNABest answer
Associate
Oct 16, 2025 6:14 AM UTC

Hello Osman,

When i update only TouchGFX to latest version (4.25.0) & keeping STM32Cube FW_H7 V1.11.2 version issue resolved.

I am using Keil IDE 5.42.0.0 & Arm_Compiler _5.06u7. 

Currently migrating to latest compiler version gives compiler error for FREERTOS. so for a time being we are using ARM_Compiler version_5.06u7.

 

Thank you very much for your hint & support.

8 replies

Osman SOYKURT
ST Technical Moderator
Aug 5, 2025 12:42 PM UTC

Hello @VNA ,

Could you provide more details about your project? 

  • Which version of TouchGFX do you use?
  • Which is the STM32H7 do you use
  • Which font do you use?
  • What's the Bpp of your typo?
  • Do you have rotated screen?
ST Software Developer | TouchGFX
VNAAuthor
Associate
Aug 6, 2025 4:21 AM UTC

Hello Osman,

Please find the details below.

- TouchGFX version - 4.21.3

- MCU STM32H757XIH6

- Font - RobNoto Medium

- Font Size-39 & Bpp - 4

- Display Orientation - Vertical - Width -480 Height-800

All other font's displayed properly, Issue is only with '5', '7'. 

 

Osman SOYKURT
ST Technical Moderator
Aug 11, 2025 2:12 PM UTC

Ok thanks for the info. First of all, I'd like to recommend you using the latest version of TouchGFX as it includes a lot of bugfixes and new feature, and it's much more easy for us to support you that way. Could you try with the latest TouchGFX?
Also could you tell if use mapped storage format or unmapped? If unmapped, try copying translations in RAM.

ST Software Developer | TouchGFX
VNAAuthor
Associate
Sep 9, 2025 11:31 AM UTC

Hello Osman,

Thank you for your inputs.

I updated to TouchGFX version 4.25.0 Font issue resolved.

Now facing new issue, Application could only run in debug mode. Earlier this problem was not there.

In startup file startup_stm32h757xx.s

VNA_0-1757416535059.png

execution up to line-245 is OK, jump to main() in application happens after pressing RUN tab multiple times in debug mode. Once execution reach main function then screen display & font all are fine.

FYI, we are using CM7 & CM4 core. use external flash QSPI & external SDRAM. Entire application was running smooth with 4.21.3 only issue we faced with fonts.

In TouchGFX -> Text configuration we enabled 

1. Remap texts,

2. A4

3. Mapped storage format.

 

Osman SOYKURT
ST Technical Moderator
Oct 9, 2025 8:39 AM UTC

Hello @VNA ,

Sorry for the late reply. Have you been able to resolve your issue?
This looks like semi-hosting issue. Which IDE are you using?

ST Software Developer | TouchGFX
unsigned_char_array
Lead III
Oct 9, 2025 9:17 AM UTC

Could be a cache issue. If you use cache do you flush your cache? You can try disabling cache.
Could also be a missing invalidate() call.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."
VNAAuthorBest answer
Associate
Oct 16, 2025 6:14 AM UTC

Hello Osman,

When i update only TouchGFX to latest version (4.25.0) & keeping STM32Cube FW_H7 V1.11.2 version issue resolved.

I am using Keil IDE 5.42.0.0 & Arm_Compiler _5.06u7. 

Currently migrating to latest compiler version gives compiler error for FREERTOS. so for a time being we are using ARM_Compiler version_5.06u7.

 

Thank you very much for your hint & support.

Osman SOYKURT
ST Technical Moderator
Oct 22, 2025 4:21 PM UTC

Hello @VNA ,

Good finding, thanks for your share. I'll check what's making the issue on the latest firmware.
Could you accept your answer as solution, so it will help the other to find the workaround at least.

Best regards,

ST Software Developer | TouchGFX