Skip to main content
AMerc.4
Senior
Jun 9, 2020 3:01 AM UTC
Question

TouchGFX error when I put a bigger image

Hello,

i can manage TouchGFX Designer with very basic objects such as an analog clock and a color background, and it works very well.

When i decided to insert a real image as background (720x720) it returns the following error during compilation:

arm-none-eabi-g++ -o "arlix3.elf" @"objects.list" -l:libtouchgfx-float-abi-hard.a -mcpu=cortex-m7 -T"C:\Users\nikte\STM32CubeIDE\workspace_1.3.0\arlix3\STM32F767IGTX_FLASH.ld" --specs=nosys.specs -Wl,-Map="arlix3.map" -Wl,--gc-sections -static -L"C:\Users\nikte\STM32CubeIDE\workspace_1.3.0\arlix3\Middlewares\ST\touchgfx\lib\core\cortex_m7\gcc" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -lstdc++ -lsupc++ -Wl,--end-group
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: arlix3.elf section `ExtFlashSection' will not fit in region `FLASH'
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: region `FLASH' overflowed by 1158828 bytes
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:74: arlix3.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.

So I thought it was a problem of the small internal flash memory. I wrote my own Quad SPI driver for W25Q256 FLASH memory, and i created a custom external loader for my custom board, which works very well with ST-LINK Utility. I can access to FLASH memory without problems.

But nevertheless the problem is always the same.

Do you know what is the problem? Thank you, Alberto.

This topic has been closed for replies.

3 replies

AMerc.4
AMerc.4Author
Senior
Jun 9, 2020 3:26 AM UTC

Ok i fixed it, but another problem appeared.

Error in final launch sequence:
 
Failed to execute MI command:
load C:\\Users\\nikte\\STM32CubeIDE\\workspace_1.3.0\\arlix3\\Debug\\arlix3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\nikte\\STM32CubeIDE\\workspace_1.3.0\\arlix3\\Debug\\arlix3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\nikte\\STM32CubeIDE\\workspace_1.3.0\\arlix3\\Debug\\arlix3.elf 
 
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation

It was uploading to the external flash, while this errore comes out. However i can erase and see my external FLASH from STM32CubeProgrammer. One strange thing is that (when it is just erased) it has all 99999999 until 0x90000400, while over there are only FFFFFFFF.

AMerc.4
AMerc.4Author
Senior
Jun 9, 2020 1:18 PM UTC

Looking at log file i think the error comes from

[41.220] spawnCubeProgrammer(): Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe

Can i upload my .elf file directly from CUBEProgrammer? I see something strange, that the .bin file is 2 GB heavy!

And the second problem it returns is

Error: failed to download Segment[1]

AMerc.4
AMerc.4Author
Senior
Jun 11, 2020 12:36 PM UTC

I don't know if the problem is my external loader (which it allows tìme to write bin files and read from QUADSPI, however i read 9999999 in the first lines), or the .ld file of my Touchgfx application.

The .ld file for the creation of the external load is

/*
*****************************************************************************
** File : linker.ld
**
** Set heap size, stack size and stack location according
** to application requirements.
**
** Set memory bank area and size if external memory is used.
**
** Target : STMicroelectronics STM32
**
*****************************************************************************
*/
 
/* Entry Point */
ENTRY(Init)
 
/* Generate 2 segment for Loader code and device info */
PHDRS {Loader PT_LOAD ; SgInfo PT_LOAD ; }
 
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM); /* end of RAM */
/* Generate a link error if heap and stack don't fit into RAM */
_Min_Heap_Size = 0x200 ; /* required amount of heap */
_Min_Stack_Size = 0x400 ; /* required amount of stack */
 
/* Specify the memory areas */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000004, LENGTH = 512K
}
 
/* Define output sections */
SECTIONS
{
 /* The startup code goes first into FLASH */
 
 .isr_vector :
 {
 	. = . + 0x1FC;
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >RAM :Loader
 
 
 
 .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) } >RAM
 .ARM : {
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 } >RAM :Loader
 
 .preinit_array :
 {
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 } >RAM :Loader
 
 .init_array :
 {
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 } >RAM :Loader
 
 .fini_array :
 {
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 } >RAM :Loader
 
 /* used by the startup to initialize data */
 _sidata = LOADADDR(.data);
 
 /* Initialized data sections goes into RAM, load LMA copy after code */
 .data : 
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 } >RAM :Loader
 
 
 /* Uninitialized data section */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss secion */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)
 
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM :Loader
 
 /* The program code and other data goes into FLASH */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 
 KEEP (*(.init))
 KEEP (*(.fini))
 
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >RAM :Loader
 
 .Dev_info :
 {
	KEEP(*Dev_Inf.o ( .rodata* ))
 } :SgInfo
 
 
 /* Constant data goes into FLASH */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >RAM :Loader
 
 
 /* User_heap_stack section, used to check that there is enough RAM left */
 ._user_heap_stack :
 {
 . = ALIGN(4);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(4);
 } >RAM :Loader
 
 
 
 
 .ARM.attributes 0 : { *(.ARM.attributes) }
}
 
 

while the .ld file of my touchgfx application is

/**
 ******************************************************************************
 * @file LinkerScript.ld
 * @author Auto-generated by STM32CubeIDE
 * @brief Linker script for STM32F767IGTx Device from STM32F7 series
 * 1024Kbytes FLASH
 * 512Kbytes RAM
 *
 * Set heap size, stack size and stack location according
 * to application requirements.
 *
 * Set memory bank area and size if external memory is used
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
 
/* Entry Point */
ENTRY(Reset_Handler)
 
/* Highest address of the user mode stack */
_estack = ORIGIN(RAM) + LENGTH(RAM);	/* end of "RAM" Ram type memory */
 
_Min_Heap_Size = 0x200 ;	/* required amount of heap */
_Min_Stack_Size = 0x400 ;	/* required amount of stack */
 
/* Memories definition */
MEMORY
{
 RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 512K
 FLASH (rx) : ORIGIN = 0x8000000, LENGTH = 1024K
 QUADSPI (r) : ORIGIN = 0x90000000, LENGTH = 32M
}
 
/* Sections */
SECTIONS
{
 /* The startup code into "FLASH" Rom type memory */
 .isr_vector :
 {
 . = ALIGN(4);
 KEEP(*(.isr_vector)) /* Startup code */
 . = ALIGN(4);
 } >FLASH
 
 /* The program code and other data into "FLASH" Rom type memory */
 .text :
 {
 . = ALIGN(4);
 *(.text) /* .text sections (code) */
 *(.text*) /* .text* sections (code) */
 *(.glue_7) /* glue arm to thumb code */
 *(.glue_7t) /* glue thumb to arm code */
 *(.eh_frame)
 
 KEEP (*(.init))
 KEEP (*(.fini))
 
 . = ALIGN(4);
 _etext = .; /* define a global symbols at end of code */
 } >FLASH
 
 /* Constant data into "FLASH" Rom type memory */
 .rodata :
 {
 . = ALIGN(4);
 *(.rodata) /* .rodata sections (constants, strings, etc.) */
 *(.rodata*) /* .rodata* sections (constants, strings, etc.) */
 . = ALIGN(4);
 } >FLASH
 
 .ARM.extab : { 
 . = ALIGN(4);
 *(.ARM.extab* .gnu.linkonce.armextab.*)
 . = ALIGN(4);
 } >FLASH
 
 .ARM : {
 . = ALIGN(4);
 __exidx_start = .;
 *(.ARM.exidx*)
 __exidx_end = .;
 . = ALIGN(4);
 } >FLASH
 
 .preinit_array :
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__preinit_array_start = .);
 KEEP (*(.preinit_array*))
 PROVIDE_HIDDEN (__preinit_array_end = .);
 . = ALIGN(4);
 } >FLASH
 
 .init_array :
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__init_array_start = .);
 KEEP (*(SORT(.init_array.*)))
 KEEP (*(.init_array*))
 PROVIDE_HIDDEN (__init_array_end = .);
 . = ALIGN(4);
 } >FLASH
 
 .fini_array :
 {
 . = ALIGN(4);
 PROVIDE_HIDDEN (__fini_array_start = .);
 KEEP (*(SORT(.fini_array.*)))
 KEEP (*(.fini_array*))
 PROVIDE_HIDDEN (__fini_array_end = .);
 . = ALIGN(4);
 } >FLASH
 
 /* Used by the startup to initialize data */
 _sidata = LOADADDR(.data);
 
 /* Initialized data sections into "RAM" Ram type memory */
 .data : 
 {
 . = ALIGN(4);
 _sdata = .; /* create a global symbol at data start */
 *(.data) /* .data sections */
 *(.data*) /* .data* sections */
 
 . = ALIGN(4);
 _edata = .; /* define a global symbol at data end */
 
 } >RAM AT> FLASH
 
 /* Uninitialized data section into "RAM" Ram type memory */
 . = ALIGN(4);
 .bss :
 {
 /* This is used by the startup in order to initialize the .bss section */
 _sbss = .; /* define a global symbol at bss start */
 __bss_start__ = _sbss;
 *(.bss)
 *(.bss*)
 *(COMMON)
 
 . = ALIGN(4);
 _ebss = .; /* define a global symbol at bss end */
 __bss_end__ = _ebss;
 } >RAM
 
 /* User_heap_stack section, used to check that there is enough "RAM" Ram type memory left */
 ._user_heap_stack :
 {
 . = ALIGN(8);
 PROVIDE ( end = . );
 PROVIDE ( _end = . );
 . = . + _Min_Heap_Size;
 . = . + _Min_Stack_Size;
 . = ALIGN(8);
 } >RAM
 
 /* Remove information from the compiler libraries */
 /DISCARD/ :
 {
 libc.a ( * )
 libm.a ( * )
 libgcc.a ( * )
 }
 
 .ARM.attributes 0 : { *(.ARM.attributes) }
 
 ExtFlashSection :
 {
 *(ExtFlashSection ExtFlashSection.*)
 *(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
 } >QUADSPI
 
	/*
 FontFlashSection :
	{
		*(FontFlashSection FontFlashSection.*)
		*(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
	} >QUADSPI
 
 TextFlashSection :
	{
		*(TextFlashSection TextFlashSection.*)
		*(.gnu.linkonce.r.*)
 . = ALIGN(0x4);
	} >QUADSPI
	*/
}