Skip to main content
YSN
Associate III
August 18, 2021
Question

TouchGFX Engine Stop / Resume to Save Power

  1. Is there any way to stop touchgfx (with DMA2D) engine and resume back after notification.
  2. Stop and Resume of Touchgfx task is not a solution as the DMA streaming is running in the background. Pls confirm ?
  3. Start / Stop / Resume the touchgfx engine to save the power as FMC/SDRAM/QSPI will also have to stall with option? Is it possible ?

This topic has been closed for replies.

1 reply

KDubo
Associate II
October 13, 2021

Hello, did you ever get a resolution on this? The only way I can get TouchGFX to resume after MCU is in STOP mode is to delete / create the TouchGFX task, which is not ideal.