Skip to main content
Associate III
Feb 29, 2024 12:56 AM UTC
Solved

TouchGFX Designer with TrustZone-enabled U5

Hi,

seems like TouchGFX Designer is unable to create a compilable folder structure for TrustZone-enabled U5 projects. So far the workaround is to use a separate non-TrustZone project and then manually sync all the changes made by TouchGFX Designer back to TrustZone-enabled one. This is very inconvenient and error-prone way to do work.

The ST stuff has been made aware of it and the answer was "We are working on it". TouchGfx version was 22.0 that time. Is there any progress on this matter?  Seems like recent TouchGFX updates didn't fix the problem.

Thanks.

This topic has been closed for replies.
LouisBBest answer
ST Employee
Mar 1, 2024 7:46 AM UTC

Hello bear2023R,

Could you tell me which version of TouchGFX you are using ? Because this issue was fixed in the 4.23.1 .

Regards,

Louis BOUDOST Software Engineer | TouchGFX

4 replies

LouisBBest answer
ST Employee
Mar 1, 2024 7:46 AM UTC

Hello bear2023R,

Could you tell me which version of TouchGFX you are using ? Because this issue was fixed in the 4.23.1 .

Regards,

Louis BOUDOST Software Engineer | TouchGFX
bear2023RAuthor
Associate III
Mar 1, 2024 3:57 PM UTC

HI LouisB,

that's indeed good news! Thanks for this. I'm using 23.0. Going to upgrade to 23.1 immediately and check it.

Thanks again

ST Employee
Mar 5, 2024 11:33 AM UTC

Hello bear2023R,

Sorry to hear that you still have issues with THREADX, I will answer you on the new thread you created.

Regards,

Louis BOUDOST Software Engineer | TouchGFX