Skip to main content
Senior III
Sep 23, 2025 6:34 AM UTC
Solved

TouchGFX Designer doesn't show the update 4.26.0

I'm seeing TouchGFX has been updated to 4.26.0 https://support.touchgfx.com/docs/miscellaneous/changelog

Unfortunately, after having launched it, no pop-up appears asking for update https://support.touchgfx.com/docs/miscellaneous/updating-to-a-new-touchgfx-version

I'm noticing even on ST Download page isn't updated https://www.st.com/en/development-tools/touchgfxdesigner.html

This topic has been closed for replies.
JohanAstrupBest answer
ST Technical Moderator
Sep 29, 2025 7:30 AM UTC

OK, then the pop-up is not for updating the TouchGFX installation; it is only for updating projects. You will get this pop-up when e.g. you open a project that is currently version 4.25.0 in version 4.26.0. As stated in the referred doc: "Simply open your newly installed version of TouchGFX Designer and try to open your older application either through recent applications or the Open dialog. You will be greeted with the following popup:".

When you press "Yes", the project will be updated to version 4.26.0. After completing this, follow the procedure below:

  1. Open STM32CubeMX and generate code.
  2. Remove all TouchGFX-generated files.
  3. Generate code in TouchGFX Designer.

Just to clarify; to get TouchGFX 4.26.0, you need to download it from one of the following links:
https://www.st.com/en/embedded-software/x-cube-touchgfx.html
https://www.st.com/en/development-tools/touchgfxdesigner.html
If you have a user account, you can log in. Then you can see 4.26.0 under "All versions". If you download it as guest, you currently need to press "Get latest".

Best regards,
Johan

6 replies

nico23Author
Senior III
Sep 25, 2025 6:33 AM UTC

Now on TouchGFX Designer a banner showing 4.26 is availble appeared but, it redirects to https://www.st.com/en/embedded-software/x-cube-touchgfx.html where 4.25 is listed at latest release.

Still, no Update pop-up as described here appears https://support.touchgfx.com/docs/miscellaneous/updating-to-a-new-touchgfx-version

ST Technical Moderator
Sep 25, 2025 6:50 AM UTC

Hello @nico23.

If you press "Download latest" in the link you have shared, you will get TouchGFX 4.26.0. I do not know why it does not currently appear under "All versions".

For the second part, are you referring to the Update TouchGFX Generator section? TouchGFX 4.26.0 is not yet directly available in STM32CubeMX. It typically takes a few weeks from the official release for it to become available on the STM32CubeMX server. You can manually install the TouchGFX 4.26.0 pack in STM32CubeMX by pressing "From Local ..." in the package manager and selecting the downloaded TouchGFX pack.

Best regards,
Johan

nico23Author
Senior III
Sep 29, 2025 6:41 AM UTC

Hi @JohanAstrup 

I'm referring to TouchGFX Designer and the pop-up described by your documentation (as linked in the previous post) that does not appear.

Thanks for the clarification. I'll wait some more time to see if the 4.26 pop-up magically appears

 

JohanAstrupBest answer
ST Technical Moderator
Sep 29, 2025 7:30 AM UTC

OK, then the pop-up is not for updating the TouchGFX installation; it is only for updating projects. You will get this pop-up when e.g. you open a project that is currently version 4.25.0 in version 4.26.0. As stated in the referred doc: "Simply open your newly installed version of TouchGFX Designer and try to open your older application either through recent applications or the Open dialog. You will be greeted with the following popup:".

When you press "Yes", the project will be updated to version 4.26.0. After completing this, follow the procedure below:

  1. Open STM32CubeMX and generate code.
  2. Remove all TouchGFX-generated files.
  3. Generate code in TouchGFX Designer.

Just to clarify; to get TouchGFX 4.26.0, you need to download it from one of the following links:
https://www.st.com/en/embedded-software/x-cube-touchgfx.html
https://www.st.com/en/development-tools/touchgfxdesigner.html
If you have a user account, you can log in. Then you can see 4.26.0 under "All versions". If you download it as guest, you currently need to press "Get latest".

Best regards,
Johan

Senior
Sep 29, 2025 3:11 PM UTC
ST Technical Moderator
Sep 30, 2025 7:31 AM UTC

Hello @Marc_LM.

I have verified again, and I can download 4.26.0 from both links if I log in.

The screenshot below is from the second link when logged in.

JohanAstrup_0-1759217372638.png

Best regards,
Johan