Skip to main content
BParh.1
Senior III
August 4, 2021
Question

TouchGFX Designer does not reflect the change in image size when overwritten

I setup a radio button using my own image instead of one provided by TouchGFFX Designer. Initial size is say 24p. But then I realize it is too small, so I override the same image file name with an image of radio button but larger size say 36p. But the TouchGFXDesigner does not reflect the change although when run, the radio button size is correct e.g. 36p.

Why this is so? Is there any hard caching used by TouchGFX? I am using v 4.17.0

This topic has been closed for replies.