Skip to main content
GS1
Senior III
Sep 23, 2025 10:46 AM UTC
Question

TouchGFX Designer does not generate Text code (Text.cpp)

 

Hi all,

Hi Martin,@Martin KJELDSEN, 

now that version 4.26.0.  of TouchGFX is out, I tried to migrate my huge project (90 screens) to this new release, but I can not get texts being generated.

What I have done:

I used the latest STM32CubeMX version (6.15.0) and regenerated code of the project with TouchGFX Version 4.26.0 selected. Then I opened TouchGFX Designer 4.26.0, migrated my project and generated code too.

There were several warnings concerning the Unicode characters like the following sample:

WARNING - Char 0xC0 is used but does not exist in the font!
WARNING - A total of 64 Unicode characters did not exist in the font!

In the first run, texts were generated correctly.

But as soon as I change a text or add a new text, these changes are no longer regenerated when pressing "Generate code".

 

Then I tried several things (proposed on a different post):

- Change all wildcard character sets from 0x20...0xFF  to 0x20...0x7E.   Did not help!

- Generate a blank (Simulator) app and imported the GUI: Text generation then works! But I need the design im my project folder, therefore:

- I then tried to import this GUI back into my original project: Text generation doesn't work then!

- I tried to generate a new (simulator) design in my current project folder and import from the working generated new project: Text generation still doesn't work.


I am out of ideas, how to fix this issue!

Can anyone tell, what is wrong and how I can fix this?

 

P.S: Version 4.24.1. ist the last working version for me. This issue arose with Version 4.25.0. already. 

Please can anyone of the employees have a look, what was changed from 4.24.1 to 4.25.0 so that these releases don't generate text anymore??

 

Thanks for help.

 

BR GS

 

    This topic has been closed for replies.

    8 replies

    ST Employee
    Sep 23, 2025 1:24 PM UTC

    Hello @GS1,

    Have you check if your project uses char 0xC0 and if your font contains it too ? You can use FontForge to check that.

    BR,

    Louis BOUDOST Software Engineer | TouchGFX
    GS1
    GS1Author
    Senior III
    Sep 23, 2025 2:02 PM UTC

    Hi Louis,

    I only use 3 font types: Calibri, CalibriB (Bold) and AbsolutDB (ABSN_.TTF)

    Using FontForge I see that both fonts should have 0xC0. This is a character which I don't use in my application (À).

    I only use the german " äöü ÄÖÜ ß " and the  "  ² " character from the calibri fonts, but these are available in the font. 

     

    Any other possible reason?

    BR

    ST Employee
    Sep 24, 2025 1:34 PM UTC

    Could you send me the fonts ?

    Louis BOUDOST Software Engineer | TouchGFX
    GS1
    GS1Author
    Senior III
    Sep 24, 2025 2:44 PM UTC

    Hi Louis,

    I have done another try, which also failed:

    I redefined the Wildcard character sets to only have 0x20 - 0x7E (instead of 0xFF).

    This eliminated the WARNING messages, however changes in the texts are still not generated.

    In Version 4.24.1 everything is working perfectly.

    I have attached a zip file with my 3 fonts.

    Hope you can find a reason... 

    BR GS

    ST Employee
    Sep 26, 2025 8:06 AM UTC

    Hello @GS1 ,

    Have you tried to delete the generated folder and regenerate ?

    BR,

    Louis BOUDOST Software Engineer | TouchGFX
    GS1
    GS1Author
    Senior III
    Sep 26, 2025 8:16 AM UTC

    Yes, I tried that. Then this folder is not regenerated.

    BR GS

     

    ST Employee
    Sep 26, 2025 8:56 AM UTC

    Can you try with different fonts (only use verdana for all your typo) ? Can you send the log output ?

    Louis BOUDOST Software Engineer | TouchGFX
    GS1
    GS1Author
    Senior III
    Sep 30, 2025 10:27 AM UTC

    After changing the Typographies of my several font sizes from Calibri to Verdana and changing the contents of 2 texts to make sure, that texts need to be generated,  the only thing that happens is as follows:

    - in the asset \ fonts folder the verdana.ttf is added 

    In the sub folder under "generated" for text and fonts:

    - text source files are not created. Previous files are untouched

    - font source files for the different typography are not created. Only the Calibri files still exist untouched.

    The log is as follows (don't know where to find a file):

    GS1_0-1759226569945.png

     

    Then I deleted the complete folder "generated" and pressed "Generate code" again.

    This should regenerate all sub-folders and files.

    But the only subfolder in "generated" now are: 

    - gui_generated

    - simulator

    and a file named user.config

     

    Missing folders: 

    - fonts

    - texts

    - images

    - videos (which I actually don't use/need) 

     

    Please note: 

    I am not using the Simulator (this is not possible in the current configuration) and therefore I deleted the command calls in the Config-build setup for the simulator creation. Same applies for the Target, because the target is created with Keil separately. The TouchGFX application is running on a custom board with 2 processors, which are loaded separately via my own lootloader into system. The 2 processors have different tasks to aquire data from CAN busses, store data to SD card and flash, etc. The 2  STM32H7A3  communicate via internal SPI ports.

    BR GS