Skip to main content
WhyIsThisSo
Associate III
Jul 16, 2022 1:57 AM UTC
Question

TouchGFX cube_programmer.mk project File template

TouchGFX projects has a cube_programmer.mk in each project folder.

I have installed my CubeProgrammer in a different location to the default location in the cube_programmer.mk. I was wondering if the cube_programmer.mk is created on each project creation as part of the code within in the TouchGFX IDE or is it a file template which is copied from another location each time? I would like to change the master file so I do not have to change the project file each time.

This topic has been closed for replies.

1 reply

MM..1
Super User
Jul 16, 2022 8:00 AM UTC

Maybe simpler is use MKLINK and create symlink on default place