Skip to main content
KMew
Senior III
Apr 14, 2023 8:17 PM UTC
Solved

TouchGFX: Creating dynamic graphic to represent Battery State of Charge (SOC)

Hello,

I am using the TouchGFX GUI on my custom board, which I have fully working now. We want to add a nicer visual display of our battery's SOC. We want a black background with a blue line that traces a hexagonal visual that changes based on the battery state of charge. The higher the state of charge, the further that the blue line "progresses." See below for a visual example.


_legacyfs_online_stmicro_images_0693W00000bi87LQAQ.png 

I can create a black box and make the text look similar to that with the right font, but I am unsure how to create those light blue lines dynamically via TouchGFX.

Does anyone have any guidance on how to do this?

This topic has been closed for replies.
ktrofimo
ktrofimoBest answer
Senior III
Apr 14, 2023 8:22 PM UTC

What about this:

Make 3 widgets the same size, on top ​of each other:

Top: text with %

Middle: black rectangle

​​Bottom: blue line bitmap

​As battery charges make middle rectangle smaller - it will open a bitmap underneath.

10 replies

ktrofimo
ktrofimoBest answer
Senior III
Apr 14, 2023 8:22 PM UTC

What about this:

Make 3 widgets the same size, on top ​of each other:

Top: text with %

Middle: black rectangle

​​Bottom: blue line bitmap

​As battery charges make middle rectangle smaller - it will open a bitmap underneath.

KMew
KMewAuthor
Senior III
Apr 14, 2023 8:35 PM UTC

Hello ktro,

Thank you for the reply!

I think I see your logic, but I am trying to picture how to write the code for what you're describing. I can make the middle rectangle smaller, but it won't be shrinking the rectangle by a certain percentage each time. What we'd need is to remove the portion of the rectangle that is "hiding" that blue line.

Would it be easier to write a code this way instead:

Top: Text with percentage AND the blue line bitmap

Bottom: Black rectangle

But for the blue line bitmap, only generate a certain percentage of it based on that SOC percentage?

ktrofimo
Senior III
Apr 14, 2023 8:45 PM UTC

Let's assume your widgets are in coordinates 0,0 to 100, 50 and Charge variable holds percentage 0 to 100. Then do in your onTick() function:​

blackBox.setPosition(Charge, 0, 100, 50);

This way ​when charge is 0% black box will fill whole area hiding blue line underneath. And it will gradually open it while charge will grow up to 100%

​

​

​

MM..1
Super User
Apr 15, 2023 11:20 AM UTC

Other idea is Image Progress | TouchGFX Documentation

or inspire Live demos - Test LVGL in your browser | LVGL Futuristic Ebike UI

click on battery

KMew
KMewAuthor
Senior III
Apr 17, 2023 3:21 PM UTC

Hello MM,

Wow, that Futuristic Ebike UI looks really fascinating! A wonderful display.

I could definitely get inspiration from that. I'm guessing a source code for that would cost money though?

MM..1
Super User
Apr 17, 2023 6:10 PM UTC

Its free example...