Solved
TouchGFX crashes on project creation
- 10 replies
- 4325 views
Hi,
I've installed TouchGFX following the instruction at https://support.touchgfx.com/docs/introduction/installation on a completely new installation of windows 10. When I try to create a project, TouchGFX crashes at 88% and simply closes. When I checked the TouchGFXDesigner.log file the error is System.IO.FileLoadException: Failed to load native freetype library!
Any idea how I can fix this?
Please see attached log file.
Thank for your help. Looking forward to get the designer working.
Richard