Skip to main content
BRobe.3
Associate III
May 4, 2023 7:05 AM UTC
Question

TouchGFX can't ru simulator

Hello,

I use ToucheGFXDesigner 4.21.3 for the first time.

I have no problem to design the application for the 2 buttoms Run Simulator and Run Target are not Highlitghted. When, I point these buttoms, it's written : Can't run Simulator and Can't run target. Samething in the menu Code

I probably miss something but what?

If somebody coul help ?

Best Regards

Robert

This topic has been closed for replies.

11 replies

BRobe.3
BRobe.3Author
Associate III
May 7, 2023 6:58 AM UTC

Hello JTP,

For your information, the issue is solved.

After your idea to cancel the 4 blocking files, I was able tu run completly TouchGFX with any project.

Then, I try to run in Stm32CubeIde. When, I open the .ioc file, the system ask for a major update (1GB). Everything was fine, I started to debug. The system ask for a firmare update of the Stm32LINK probe ( included in the board).

After that, I run the project from Stm32CubeIde. Everything was fine and the demo is perfect on the board.

Then, I redo the TouchGFX simulation. The 4 blocking files are no more blocking.

My understanding now is the firmware update of the Stm32LINK probe is the key point.

Thanks again for your support

Best regards