Skip to main content
CPaye.1
Associate III
December 13, 2021
Solved

Touchgfx bulleted text list?

I have an application where there is a potential for lots of text. It would be nice to break up the next into a bulleted list or a numbered list. Is there a clever way to do this with the Touchgfx framework?

I think making typed text values for each block will be too tedious for the amount of text I will be working with. The only other option I can think of is creating an image of the formatted text and using that.

Thanks.

This topic has been closed for replies.
CPaye.1
CPaye.1Best answer
Associate III
December 21, 2021

It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application:

0693W00000HpOhdQAF.png

2 replies

MM..1
Super User
December 18, 2021

Maybe nobody understand without example, try show one or two onscreen texts

CPaye.1
CPaye.1AuthorBest answer
Associate III
December 21, 2021

It turns out that if you use bulleted text in the Excel spreadsheet, that bullets will carry over into the text generated for the application:

0693W00000HpOhdQAF.png