Skip to main content
ANauz.1
Senior
Jan 30, 2023 2:57 PM UTC
Question

TouchGFX application is blocking FreeRTOS-Plus-TCP

I have a projet with FreeRTOS and FreeRTOS-Plus-TCP working on a STM32F769I-Eval board.

The ICMP Ping response is 100%.

When enabling a TouchGFX application, even very basic (just a white screen), the ping response rate fall bellow 50%! Not usable at all!

Deactivating the TouchGFX application (comment on the line creating the thread) solve the Ping problem.

Is there a compatibility problem with TouchGFX and ETH on the board?

Or does anybody knows what could explain this behavior?

TouchGFX version 4.21, F7 Firmware v1.17.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Feb 7, 2023 5:10 PM UTC

Hello @ANauz.1​,

Did you start from scratch (from TouchGFX Designer) or from STM32CubeMX?

It maybe you have an issue with Ethernet/FreeRTOS config! Can you share the settings?

Refer to these posts with Ethernet issues:

Take a look at this video. It might help you.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks