Skip to main content
TSour.1
Associate II
May 9, 2022 2:26 PM UTC
Question

TouchGFX and UART sending data

Hello,

I'm working in touchgfx with STM32F469I discovery, i'm trying to communicate with PC using UART function.

I used this tuto : (1) TouchGFX - sending uart data to GUI on a STM32F746G-DISC0 - YouTube

i'm using RealTerm TCP/IP to send data, but it doesn't work.

you can find the code in Github : ISSUE WITH SENDING DATA BY UART TO VIEW · GitHub

Can anyone help me please !

Thanks,

This topic has been closed for replies.

8 replies

MM..1
Super User
May 9, 2022 8:14 PM UTC

TCP/IP???

What is your error? Debug your code simulate data receive first...

TSour.1
TSour.1Author
Associate II
May 10, 2022 7:39 AM UTC

Thank you for your response,

I’m sorry I mean: RealTerm: Serial/TCP terminal

I have no errors with the code, but the data is not displayed on the screen.

Angle
Associate III
Dec 21, 2022 6:38 AM UTC

Hi, did you able solve the problem? im facing the same problem right now

MM..1
Super User
May 10, 2022 4:30 PM UTC

Im not expert for semaphore, MVP system use queues , but simple i repeat. DEBUG your code:

  1. Is UART received to buffer ?
  2. Variable triggered ?
  3. ...
nsabo.1
Associate III
Dec 20, 2022 7:55 AM UTC

Hi, I have the same problem.

I set a screen page to transmit and receive UART data , but nothing happens

can you tell me how to check the variable in debug?

I don't know how to it...

I am beginner.

Thanks.

MM..1
Super User
Dec 20, 2022 3:20 PM UTC

Open new ticket and show code, but primary UART cant be handled in screen or model, you require separate thread. Maybe can in nonblockin mode handling...

Karl Yamashita
Super User
Dec 20, 2022 9:06 AM UTC

Are you sure you're receiving data? Did you enable global interrupt for UART6 in NVIC configuration?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source