Skip to main content
Associate II
Aug 6, 2024 7:31 AM UTC
Solved

Touchgfx and HAL_GPIO_WritePin in simulator

This piece of code works if I transfer it to my board, but if I use the simulator in TouchGFX, I get an error: gui/src/model/Model.cpp:7:10: fatal error: main.h: No such file or directory #include "main.h".
 
Screen1View.cpp
#include "stm32f7xx_hal.h"
 
// LED Toggle function
void Screen1View::ToggleLED()
{
 if (toggleButton1.getState()) HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
 else HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
}
 
I am using TouchGFX 4.24
BR 
This topic has been closed for replies.
unsigned_char_array
Lead III
Aug 9, 2024 8:18 AM UTC

@LouisB wrote:

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

 


extern C is not needed as stm32f7xx_hal.h already has this inside the header file. As far as I know all ST header files are like this.

 

This would work:

 

#ifndef SIMULATOR
#include "stm32f7xx_hal.h"
#endif

// LED Toggle function
void Screen1View::ToggleLED()
{
	if (toggleButton1.getState())
	{ 
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
	else
	{
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
}

 

 

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."

7 replies

amigafanAuthor
Associate II
Aug 6, 2024 10:28 AM UTC

Ups, the error is:gui/src/model/Model.cpp:7:10: fatal error: stm32f7xx_hal.h: No such file or directory #include "stm32f7xx_hal.h". Sorry

ST Employee
Aug 6, 2024 3:14 PM UTC

Hello @amigafan ,


How did you include the file in your project ? The board and the simulator are built differently.

 

Best regards,
Louis B.

Louis BOUDOST Software Engineer | TouchGFX
amigafanAuthor
Associate II
Aug 6, 2024 3:27 PM UTC

?? I wrote #include "stm32f7xx_hal.h" in Screen1View.cpp.

Br

ST Employee
Aug 6, 2024 3:33 PM UTC

I meant in which folder did you put the file ?

Louis BOUDOST Software Engineer | TouchGFX
amigafanAuthor
Associate II
Aug 6, 2024 3:39 PM UTC

It is in STM32CubeIDE, I dit no add a file to any folder.

ST Employee
Aug 9, 2024 7:27 AM UTC

Hello @amigafan,

The issue is the file itself, it's an hardware specific file that will only work on target.

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

I hope it helps,
Best regards

Louis BOUDOST Software Engineer | TouchGFX
unsigned_char_array
Lead III
Aug 9, 2024 8:18 AM UTC

@LouisB wrote:

 

#ifdef SIMULATOR

 // Your simulator specific user code here

 #include "gui/common/myInclude.hpp"

#else
 // Your hardware specific user code here

 extern "C"

 {

 #include "stm32f7xx_hal.h"

 }

#endif
 

 

 


extern C is not needed as stm32f7xx_hal.h already has this inside the header file. As far as I know all ST header files are like this.

 

This would work:

 

#ifndef SIMULATOR
#include "stm32f7xx_hal.h"
#endif

// LED Toggle function
void Screen1View::ToggleLED()
{
	if (toggleButton1.getState())
	{ 
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
	else
	{
		#ifndef SIMULATOR
		HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);
		#else
		//simulate an LED on the screen, for example
		#endif
	}
}

 

 

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."