Skip to main content
Associate II
Sep 7, 2025 3:17 AM UTC
Question

TouchGFX 4.25 cannot run .

 It is compiled with AC6.24 in MDK 5.43.

run on NUCLEO-H7A3ZI-Q.

But it cannot run.

compiling is ok. 

The programme compiled with stm32cubeIDE is not problem.It can run perfectly.

The project is attached blow.

This topic has been closed for replies.

2 replies

ST Employee
Sep 9, 2025 7:15 AM UTC

Hello @magicmatrix,

What error messages do you have ? Did you try to debug in Keil, if so where is your program stuck ?

BR,

Louis BOUDOST Software Engineer | TouchGFX
Associate II
Sep 10, 2025 8:33 AM UTC

After adding the touchgfx library to the program.The program will halt at the three "bkpt" instructions.

see attached file.

I think the instructions is in the c runtime library.

Is it the case that the runtime library of the new compiler and the touchgfx library are incompatible?

Is it necessary to try recompiling the touchgfx library using the new version of the compiler?