Skip to main content
stst9191
Associate II
Mar 24, 2023 7:52 AM UTC
Solved

TouchGFX 4.21, Position of text in Button With Label

The new version of TouchGFX (V4.21.0, V4.21.1) displays the text of a Button With Label no more vertical centered. In the designer the text is shown correctly, but in the simulator and in the compiled controller application it is positioned too high.

Is there a way to correct the position?

0693W00000aJdHiQAK.bmpScreenshot with TouchGFX 4.20.0

0693W00000aJdKHQA0.bmpScreenshot with TouchGFX 4.21.1

This topic has been closed for replies.
Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Mar 24, 2023 10:51 AM UTC

Hello @stst9191​,

We modified the way we position the text inside the Button with Label between v.4.20.0 and v.4.21.0.

We did those changes to reposition the label text if the font includes a character that goes lower that the font baseline, for example "g".

If you want to get the same behavior as before, you can modify the updateTextPosition() inside the touchgfx\framework\include\touchgfx\widgets\ButtonWithLabel.hpp file inside your project.

You can modify text height spacing by replacing getHeight() by getMaxTextHeight(), like this :

0693W00000aJeBaQAK.pngAlso, since getMaxTextHeight() is now a deprecated method, you'll also have to remove the deprecation tag inside the touchgfx\framework\include\touchgfx\Font.hpp file :

0693W00000aJeCEQA0.png 

FYI, we are discussing this internally and considering the fact to add a method or functionality to enable the user to modify the position of the label inside the button by himself.

Hope that helps,

/Yoann

Yoann KLEINST Software Developer | TouchGFX

4 replies

Yoann KLEIN
Yoann KLEINBest answer
ST Employee
Mar 24, 2023 10:51 AM UTC

Hello @stst9191​,

We modified the way we position the text inside the Button with Label between v.4.20.0 and v.4.21.0.

We did those changes to reposition the label text if the font includes a character that goes lower that the font baseline, for example "g".

If you want to get the same behavior as before, you can modify the updateTextPosition() inside the touchgfx\framework\include\touchgfx\widgets\ButtonWithLabel.hpp file inside your project.

You can modify text height spacing by replacing getHeight() by getMaxTextHeight(), like this :

0693W00000aJeBaQAK.pngAlso, since getMaxTextHeight() is now a deprecated method, you'll also have to remove the deprecation tag inside the touchgfx\framework\include\touchgfx\Font.hpp file :

0693W00000aJeCEQA0.png 

FYI, we are discussing this internally and considering the fact to add a method or functionality to enable the user to modify the position of the label inside the button by himself.

Hope that helps,

/Yoann

Yoann KLEINST Software Developer | TouchGFX
SWT-GAL
Associate II
Jun 4, 2024 6:06 AM UTC

Hi Yoann

Thank you for your answer, that helps. I ran into the exact same situation when upgrading from 4.20 to 4.23.2. Are there any plans to make this configurable (or even automated) in the future? Like the OP already stated the pre-4.21.1 is the preferred solution e.g. in case there's only capital letters or numbers.

Thanks,
Lukas

stst9191
stst9191Author
Associate II
Mar 24, 2023 11:21 AM UTC

Hello Yoann,

thank you for your help. I have made your suggested modifications and it works with the same behavior as before (that I prefer in this application).

/Stefan

Associate II
Jun 6, 2025 6:25 AM UTC

Hello, I think the above workaround is no longer possible with current TouchGFX 4.25.0, as the getMaxTextHeight function is not present anymore.

 

Are there other workarounds available?