Skip to main content
SMark.3
Associate
May 19, 2021
Question

TouchGFX 4.15 puts incorrect Library Search Path into .cproject file

When I generate code on my TouchFGX 4.15.0 project, it overwrites the correct Library Search Path in my STM32CubeIDE .cproject file and replaces it with this one:

"${workspace_loc:/Executable/Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc}}"

In fact the correct location for the library is:

"${workspace_loc:/${ProjName}/Middlewares/ST/TouchGFX/touchgfx/lib/core/cortex_m7/gcc}"

I can't find any way to change this in the .touchgfx file or elsewhere. How can I correct this so I don't need to manually change every time I regenerate the code?

This topic has been closed for replies.

4 replies

SMark.3
SMark.3Author
Associate
May 27, 2021

Anyone? @Martin KJELDSEN​  can you help with this?

Romain DIELEMAN
ST Employee
May 27, 2021

Hi,

Do you also face this issue with TouchGFX 4.16.1 ? How did you create your project ? Was it from scratch or did you use an application template for one of ST development kits ?

/Romain

SMark.3
SMark.3Author
Associate
May 27, 2021

Hi,

I haven't tried with 4.16.1, still running 4.15. I originally created my project when TouchGFX was first introduced into CubeMX - I think TouchGFX Version 4.10 or similar. I used the code generator to create the project. It started to behave badly after migrating to V4.15.

Martin KJELDSEN
Principal III
May 27, 2021

Hi. Pretty sure we fixed something like that in the following releases. It's not a configuration you'll find in the .project file. It happens during post-generation to include all the right files in your projects.

I could point you to the ruby scripts that modify this path inside the installed TouchGFX Environment if you want to have a look. Maybe we'll provide a patch for you.

/Martin