Skip to main content
scottSD
Senior III
December 15, 2020
Question

TouchGFX 4.15.0 L8 conversion is different than TouchGFX 4.14.0.

Has something in the image conversions changed in TouchGFX 4.15.0?

I was surprised that one of my images being converted to an L8_ARGB8888 failed when doing a conversion in the Designer. The image in question had only 201 colors, but when doing a GENERATE in the Designer, it failed, telling me the image couldn't be converted because it had 584 colors. The image does have alpha.

I tried this same image conversion in TouchGFX 4.14.0 with the same dithering setting and it converted it fine.

This topic has been closed for replies.

1 reply

JP11
Visitor II
December 17, 2020

Hi there!

Just stumbled over a similar problem - picture with 128 colors, but error: "too many colors". Solved it by disabling dithering.

hth