Skip to main content
Kasun Dinesh
Associate III
Jan 21, 2020 4:46 PM UTC
Solved

Touchgfx 4.13 and Cubemx 5.5 project creation

Hi,

I use the .ioc file in STM32F746-DISCO v.3.0.0 project, import it to CUBE IDE and used the option to create a project form ioc file. But even i compiled and run in in stm32f746 board, nothing happens. Any reason for this, or whats the fix. My end goal is to make it compatible with a display of 800x480.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jan 23, 2020 10:39 AM UTC

But did you actually program the flash with the contents of this region? You require an external flashloader configured from either ST-Link or STCubeProgrammer - Or through CubeIDE.

8 replies

Martin KJELDSEN
Principal III
Jan 21, 2020 9:12 PM UTC

"Nothing happens" - Can you elaborate?

Kasun Dinesh
Associate III
Jan 22, 2020 3:07 AM UTC

Nothing comes to display. I created a gui in touchgfx. Build it using new cubeide but when I run it, nothing comes to the display. ​there are no errors or hard faults comes when running.

Kasun Dinesh
Associate III
Jan 23, 2020 10:11 AM UTC

Hi Martin. Thanks for getting back to me. I use the default images provided from touchgfx and it's in quadspi region. I used the linker modifications done in the example project generated from touchgfx for f746​

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Jan 23, 2020 10:39 AM UTC

But did you actually program the flash with the contents of this region? You require an external flashloader configured from either ST-Link or STCubeProgrammer - Or through CubeIDE.

Kasun Dinesh
Associate III
Jan 23, 2020 2:52 PM UTC

Thanks. That was the issue. It worked after i added the flash loader. :grinning_face: