Skip to main content
Miguel Moran
Associate II
Jul 9, 2019 3:21 PM UTC
Question

TouchGfx (4.10.0) in CubeMX (5.2.1) & Keil (5.25.2)

I have had problems to integrate TouchGfx (4.10.0) in CubeMX (5.2.1) & Keil (5.25.2), I have followed all the steps in detail that are on your page, following the steps for this purpose and the button EXE is not enabled. What should I do? Is there another way to integrate the 3 tools?

This topic has been closed for replies.

11 replies

Martin KJELDSEN
Principal III
Jul 9, 2019 3:28 PM UTC

Hi @Miguel Moran​,

I need some additional information. did you install Touchgfx 4.10.0 and point CubeMX to the designer executable? Did you "generate code" at least once? (Otherwise the .touchgfx project file won't be generated and the designer can't open anything).

Thanks!

Best regards,

Martin

Miguel Moran
Associate II
Jul 9, 2019 3:41 PM UTC

I have already installed the cubeMX software and I have used it with Stemwin for some time now, without any problem, I always keep the CubeMX & Keil updated. I have installed Touchgfx, from the CubeMx pack folder, I have carefully followed the configuration instructions, which are suggested on your page and I have compiled the project at least once as indicated.

Miguel Moran
Associate II
Jul 9, 2019 3:40 PM UTC

.