Skip to main content
patrickschneider9
Associate III
Apr 25, 2022 12:33 PM UTC
Solved

TouchGFX 180 degree orientation?

Hi everyone,

is it somehow possible to "flip" the screen for a 180 degree rotation?

Either on TouchGFX, LTDC or DMA2D level?

We are using CubeMX to generate the whole project and everything works smoothly, but we need to rotate the screen.

Cheers,

Patrick

This topic has been closed for replies.
Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 25, 2022 2:34 PM UTC

Unfortunately, it is not yet possible to realise this in TouchGFX. As a rule, users have so far developed the graphic interface for a static system and in such a case simply rotated the entire display by 180 degrees, i.e. mechanically. You may be able to do the rotation at driver level because some displays allow that. 

However, there is a thread here in the community in which a software solution with all its disadvantages has already been discussed.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

3 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 25, 2022 2:34 PM UTC

Unfortunately, it is not yet possible to realise this in TouchGFX. As a rule, users have so far developed the graphic interface for a static system and in such a case simply rotated the entire display by 180 degrees, i.e. mechanically. You may be able to do the rotation at driver level because some displays allow that. 

However, there is a thread here in the community in which a software solution with all its disadvantages has already been discussed.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
patrickschneider9
Associate III
Apr 25, 2022 3:34 PM UTC

Hello Peter,

thanks for pointing me to this thread!

MSale.1
Senior
Aug 29, 2023 11:38 AM UTC

@patrickschneider9 

The main problem in 90 degree rotation with DMA2D is that it lacks the ability to decrement the destination address. there is an optimized way to rotate an image 90 degree with much better performance compared to software version.

for 180 degree you can use MDMA. they have an example for it.

Regards

M.Salem