Skip to main content
Associate III
Jan 22, 2025 12:56 PM UTC
Question

TouchGFX

HI,

I have a Touch GFX-based application with External Quad SPI flash integrated for Assets, such as images and font. The Application code has more than 150 Screens Due to this internal flash is running out of memory, Even though we are using 0s optimization for GCC there is internal flash memory scarcity.  Is there any way I can place the Application code of Touch GFX in the External Flash using keywords like 

Place part of code on external flash ____attribute__((section(".name") 

Thanks and Regards 

JIJO

This topic has been closed for replies.

1 reply

urbito
Senior II
Jan 22, 2025 1:05 PM UTC

You can put all your code in QSPI and create a program in internal memory to jump to it.

 

Greetings