Skip to main content
Vins
Associate III
Sep 21, 2022 5:23 AM UTC
Question

Touch GFX with SPI Display.

Hi Community,

I have followed the following link https://www.youtube.com/watch?v=suMytEyQTP4&t=774s and got the output (SPI display interfacing with Touch GFX). Now I wanted to use the single framebuffer strategy to get the same but no output. So, anyone knows what to do with the single framebuffer strategy?

/Vins

This topic has been closed for replies.

2 replies

Osman SOYKURT
ST Technical Moderator
Sep 22, 2022 8:39 AM UTC

Hello Vins,

Could you give more information about your configuration please ?

  • Which board do you use ? Are you using a TouchGFX Board Setup or did you start your project from scratch?
  • Which version of TouchGFX Designer do you use ?
  • Which version of STM32CubeMX do you use ?

I've made a quick tutorial about how to enable double buffering strategy with DSI displays. So I guess if you revert the changes I did on the tutorial, you'll have get your board using a single framebuffer strategy.

/Osman

ST Software Developer | TouchGFX
Vins
VinsAuthor
Associate III
Sep 23, 2022 5:03 AM UTC

Hi @Osman SOYKURT​ 

My configurations.

  1. Custom Board -STM32F769AIY6TR. and I started from the scratch
  2. Touch GFX Version -4.20.2
  3. CubeMX-6.6.1.
  4. CubeIDE-1.10.1.

I am using SPI display. As per the video I got the output for partial framebuffer, but not getting the output for single framebuffer.