Skip to main content
KGlei.1
Visitor II
Jan 16, 2020 6:12 AM UTC
Question

Touch GFX on STM32F469 or STMF769 Boards with Resolution 1280x720

Hi at all,

we want to use Touch GFX for our display project. Actually we use a display with rgb interface.

Now i have seen, that the newer STM32 boards with F469 and F769 are using a DSI (MIPI) interface to the display and it is always the 4" 800x480 mounted.

Touch GFX supports these boards with demo projects. Now i want to know:

1) We want to use a 5" display and these with DSI. These types use a resolution of 1280x720.

Is it possible to reconfigure the demo project, that it will work with it?

2) What must be reconfigured in the demo project?

Thanks,

Korbinian

This topic has been closed for replies.

1 reply

Martin KJELDSEN
Principal III
Jan 16, 2020 8:41 AM UTC

Hi @KGlei.1​,

1) Depending on what you want to do, and the bitdepth of your application, you'll find any DSI-capable MCU from ST having a hard time with that many pixels. 800x480 is a stretch as it is now, even for an F769 using full screen transitions in 24bpp. So consider that.

2) You'll need to configure the LTDC+DSI HOST a bit differently, and configure the TouchGFX HAL slightly different as well since the drivers we use are, as you say, for 800x480. It's a matter of splitting the framebuffer into sections that are transferred one at a time until the entire framebuffer is sent.

The TouchGFX DSI driver itself will probably work as it is with your new display.

Let me know when you get closer.

/Martin