Skip to main content
Associate III
Feb 21, 2025 11:58 AM UTC
Question

Touch GFX debug issue

Hello,

I have integrated touch GFX with quad SPI, and images are stored in external flash, in debug mode the code is getting stuck inside the Hal Delay. What is the root cause for this, if I disable the external loader the Hal delay does not get stuck.

 

 

This topic has been closed for replies.

5 replies

GaetanGodart
ST Employee
Feb 21, 2025 1:32 PM UTC

Hello @jijomathew ,

 

Have you bene able to fix your previous issue ?

 

Can you share the call stack like you did in your previous issue so we can all investigate where it is stuck exactly?

It does sound like an issue with the external loader exclusively, have you been able to make it work previously?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
Feb 24, 2025 9:18 AM UTC

Hello @jijomathew ,

 

Great to hear!

Can you give us more information on the current issue so we can help you better?

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
Associate III
Feb 25, 2025 6:09 AM UTC

Hello,

 

I am using External loader to put Assets inside the external QSPI flash, once  I use Hal Delay inside  my code , in debug mode the code is stuck inside the Hal Delay. if I disable the Loader file in debug configuration the code is working fine. what will be the root cause and how I can trouble shoot

 

 

Associate III
Mar 4, 2025 6:53 AM UTC

quad.png

This is my debugger configuration for the Quad SPI external loader. Once I tick Initialize the Quad SPI, and if I debug the code, it gets stuck in HAL delay. is this a Debugger Configuration issue or a Loader file issue? Please help me to overcome this issue