Skip to main content
jumman_JHINGA
Senior III
Feb 26, 2025 6:15 AM UTC
Solved

Touch Display getting flicker when data is getting updated through TouchGFX task

Hello Friends.

 

Now i have started working on bigger display with TouchGFX Custom Boards. Im using 10.1 inch 1024x600 touch display. using QUADSPI,SDRAM, FMC and LTDC.

 

Through TouchGFX Designer i taken one backgoround image, one Text Area buffer and one Digital clock. when im not updating digital clock data and text area im  getting proper display.

Nor.jpeg

but when i starts updating digital clock in void screenView::handleTickEvent() then my display starts flickering and white lines appearing on display.

FL.jpegFL2.jpeg

 

my LTDC configuration:

void MX_LTDC_Init(void)
{

 /* USER CODE BEGIN LTDC_Init 0 */

 /* USER CODE END LTDC_Init 0 */

 LTDC_LayerCfgTypeDef pLayerCfg = {0};

 /* USER CODE BEGIN LTDC_Init 1 */

 /* USER CODE END LTDC_Init 1 */
 hltdc.Instance = LTDC;
 hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
 hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
 hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
 hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
 hltdc.Init.HorizontalSync = 40;
 hltdc.Init.VerticalSync = 9;
 hltdc.Init.AccumulatedHBP = 200;
 hltdc.Init.AccumulatedVBP = 29;
 hltdc.Init.AccumulatedActiveW = 1224;
 hltdc.Init.AccumulatedActiveH = 629;
 hltdc.Init.TotalWidth = 1384;
 hltdc.Init.TotalHeigh = 659;
 hltdc.Init.Backcolor.Blue = 0;
 hltdc.Init.Backcolor.Green = 0;
 hltdc.Init.Backcolor.Red = 0;
 if (HAL_LTDC_Init(&hltdc) != HAL_OK)
 {
 Error_Handler();
 }
 pLayerCfg.WindowX0 = 0;
 pLayerCfg.WindowX1 = 1024;
 pLayerCfg.WindowY0 = 0;
 pLayerCfg.WindowY1 = 600;
 pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
 pLayerCfg.Alpha = 255;
 pLayerCfg.Alpha0 = 0;
 pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_PAxCA;
 pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_PAxCA;
 pLayerCfg.FBStartAdress = 0xD0000000;
 pLayerCfg.ImageWidth = 1024;
 pLayerCfg.ImageHeight = 600;
 pLayerCfg.Backcolor.Blue = 0;
 pLayerCfg.Backcolor.Green = 0;
 pLayerCfg.Backcolor.Red = 0;
 if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN LTDC_Init 2 */

 /* USER CODE END LTDC_Init 2 */

}

 

my FMC configuration:

void MX_FMC_Init(void)
{
 /* USER CODE BEGIN FMC_Init 0 */

 /* USER CODE END FMC_Init 0 */

 FMC_SDRAM_TimingTypeDef SdramTiming = {0};

 /* USER CODE BEGIN FMC_Init 1 */

 /* USER CODE END FMC_Init 1 */

 /** Perform the SDRAM1 memory initialization sequence
 */
 hsdram1.Instance = FMC_SDRAM_DEVICE;
 /* hsdram1.Init */
 hsdram1.Init.SDBank = FMC_SDRAM_BANK2;
 hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
 hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
 hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16;
 hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
 hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
 hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
 hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
 hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
 hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1;
 /* SdramTiming */
 SdramTiming.LoadToActiveDelay = 2;
 SdramTiming.ExitSelfRefreshDelay = 7;
 SdramTiming.SelfRefreshTime = 4;
 SdramTiming.RowCycleDelay = 6;
 SdramTiming.WriteRecoveryTime = 2;
 SdramTiming.RPDelay = 2;
 SdramTiming.RCDDelay = 2;

 if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
 {
 Error_Handler( );
 }

 /* USER CODE BEGIN FMC_Init 2 */
 FMC_Bank1_R->BTCR[0] &= ~FMC_BCRx_MBKEN;
 BSP_SDRAM_Init();
 /* USER CODE END FMC_Init 2 */
}

i dont have a idea whats going wrong with this display. if any one knows please help to resolve this issue.

This topic has been closed for replies.
jumman_JHINGA
jumman_JHINGABest answer
Senior III
Mar 12, 2025 12:36 PM UTC

Im happy to inform you guys that my issue got resolved!..

There is some issue present in the  External crystal Frequency (HSE) , Instead of HSE i taken HSI and its starts working correctly.   

16 replies

jumman_JHINGA
Senior III
Mar 10, 2025 6:08 AM UTC

hii @INaee.1  i already tried 20 MHZ to 70 MHZ LTDC frequencies best output but with less flickering im getting at 37.5MHZ  as im increasing the frequency flickering increases even more.

INaee.1
Associate II
Mar 10, 2025 6:26 AM UTC

Hi ,

which LVDS serializer you have used ?

I.N

jumman_JHINGA
Senior III
Mar 10, 2025 6:37 AM UTC

im using direct RGB parallel interface. im doubting on display, beacuse colors of image are not apearing same as compare to ToucGFX designer image. e.g. in TouchGFX the image is dark Blue with Gray shades, but on LCD it apears completly light blue without gary shades.

 

im searching alternative display with same size and same pin mapped connector.

jumman_JHINGA
jumman_JHINGAAuthorBest answer
Senior III
Mar 12, 2025 12:36 PM UTC

Im happy to inform you guys that my issue got resolved!..

There is some issue present in the  External crystal Frequency (HSE) , Instead of HSE i taken HSI and its starts working correctly.