Skip to main content
TLaur.3
Associate II
Dec 12, 2022 10:43 AM UTC
Question

Touch Controller Board Reference

Hi,

I'm currently working on the STM32H753I-EVAL02 with the 5.7" parallel RGB 24 screen.

Now, I would like to buy a bigger screen with higher resolution (e.g. 7/8" - 1024*600). With this configuration, it's recommended to use LVDS rather than parallel RGB.

So, for that, I will need a new controller board that takes for input parallel RGB 24 (from the motherboard) with a 50 pins IDC connector and for output, LVDS.

After long research, I don't find any controller board that matching this case.

Does anyone have some references (or just one ! :D) ? Or does someone have never changed a parallel RGB touch screen by an LVDS ?

Thanks

This topic has been closed for replies.