Associate II
May 7, 2025 5:53 AM UTC
Question
TFT interface with stm32U5VJT6, TouchGFX via FMC Parallel RGB Interface
- 2 replies
- 763 views
I am currently working on interfacing a 2.83-inch TFT display (320x240 resolution) with the STM32U5F7VJT6 microcontroller using the FMC parallel 8080 interface. I have successfully configured the FMC in STM32CubeMX with the following settings:
-
Mode Configuration: NOR Flash/PSRAM/SRAM/ROM/LCD1
-
Chip Select: NE1
-
Memory Type: LCD Interface
-
LCD Register Select: A16
-
Data Width: 16 bits
After generating the code, I utilized the ST7789 driver to fill the screen with solid colors using the function ST7789H2_FillRect(0, 0, 320, 240, 0xFFFF);, which worked as expected.
Subsequently, I aimed to integrate TouchGFX to enhance the graphical interface. I configured TouchGFX accordingly, added an image using ApplicationTemplate.touchgfx.part, generated the code, and flashed it to the device. However, the image does not appear on the TFT display.
I would appreciate your guidance on the following:
-
TouchGFX Integration: Are there specific steps or configurations required to ensure TouchGFX operates correctly with the FMC parallel RGB interface?
-
Display Initialization: Could there be additional initialization required for the ST7789 controller when used with TouchGFX, so that assets showing properly on the display?
-
Debugging Steps: What would be the recommended approach to debug and identify the root cause of the image not displaying?