Skip to main content
AJT141
Associate III
Oct 27, 2020 2:06 PM UTC
Solved

Textearea glitches (touchgfx)

Hello,

I'm currently developing an application on a STM32H753VT6 with touchGFX and I have an issue with textAreas. Just to say that I'm using my personnal font ( size : 20/24/34 px). Each textArea has just one wildcard with a 17 chars size buffer. I'm sending text through a terminal on my PC to change wildcards values.

In some cases, I don't know when, one letter is not totally displayed even if I invalidate all possible areas. Here are some pictures to illustrate the problem :

0693W0000059ikzQAA.jpg0693W0000059ilFQAQ.jpg0693W0000059ij9QAA.jpgAs you can see, it is always the second character that is partially displayed (but sometimes there is no problem, for example, adding a space " " before "APPEL EN COURS" works)

Any idea ?

Regards,

AJT

This topic has been closed for replies.

4 replies

Romain DIELEMAN
ST Employee
Oct 28, 2020 11:14 AM UTC

Hi,

Could you share your font and your code handling the texts? Does that issue happen with other fonts as well?

/Romain

AJT141
AJT141Author
Associate III
Oct 28, 2020 11:52 AM UTC

Hello,

Here there are.

Search when strncpy function is used in cpp files to see where texteAreas are updated

And yes I've juste tried with the Courier New Font (size : 34) and I have the same problem with 16 W (the 2nd one is not totally displayed) (test done for the the call in progress screen)

Thnks again,

AJT

Associate
May 14, 2024 10:29 AM UTC

Hi there

I have been trying to follow the above link, as I am experiencing the same problem, with parts of text appearing erased.  However, when I click on the link given, I get:

"An invalid set of parameters has been specified in the url."

Could you please repost a valid link (I know that the original one is a few years old now)?

Many thanks,

John