Skip to main content
Associate III
Apr 20, 2024 2:24 PM UTC
Solved

TextArea doesnt show any text

I tried to show text via textArea, i put some string into translation field, i see the string in designer but when i ran it the text is not present. I tried similar thing with digital clock with same result. I tried define own typographies with or without wildccards and non generated texts but all with the same result. I tried it on real hardware, other things like images and buttons are visible but the text in textArea not. Should i call some method for rest of init textArea?

This topic has been closed for replies.
Petr3Best answer
Associate III
Apr 20, 2024 8:24 PM UTC

Now it works! I unchecked Binary font files box in Config -> Text Configuration and all texts are visible in simulator and hardware.

5 replies

mƎALLEm
ST Technical Moderator
Apr 20, 2024 2:29 PM UTC

Hello,

Did you call:

textArea.invalidate();

 after setting the string?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Petr3Author
Associate III
Apr 20, 2024 4:54 PM UTC

No, i put initial value in the TouchGFX Designer only. I didn't change the string by my custom firmware yet. I can try call that in the method screenView::setupScreen()

MM..1
Super User
Apr 20, 2024 6:20 PM UTC

TouchGFX version?