Tell me how to use it simply. setBitmaps (const Bitmap & bitmapReleased, const Bitmap & bitmapPressed)
There is an image button.
In Normal state, the image is displayed, and when the button is pressed, the B image is displayed.
I looked at the functions to use this function.
setBitmaps (const Bitmap & bitmapReleased, const Bitmap & bitmapPressed)
If you use this function to set the boolean bpressInfo to zero.
bitmapReleased displays A image, bitmapRressed displays B image.
And if bpressInfo is 1, bitmapReleased is B image and bitmapRressed is A image.
If the function is possible, can you show me a simple example?