Skip to main content
Associate II
Jul 18, 2025 9:51 AM UTC
Question

Swipe container with ClickListener for each page

Hello,

I've implemented, using the Designer, a Swipe container composed by 2 pages which are respectively 2 containers (SwipeContainerPage1, SwipeContainerPage2).

Each page includes some text and box which are updated on page swipe change and everything works fine.

Now I want to command an Action (a page change) when the user presses for a couple of seconds (let's say 2 seconds) SwipeContainerPage1 or SwipeContainerPage2 while maintaing the swiping property of this macro object.

Is this possible? I've taken as a reference the "ClickListener_Implementation_longPress" as a reference but with no success...

(Edited) I tried doing this and it works for the first page (calls goTo_GUITemperatureSet_Action()) but it blocks the swipe capability and I cannot go to the SwipeContainerPage2:

//In the .hpp file
class GUIMainSwipe_View : public GUIMainSwipe_ViewBase
{
public:
 GUIMainSwipe_View();
 virtual ~GUIMainSwipe_View() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 virtual void handleTickEvent();

 //container click handler
 void containerClickHandler(const Container& c, const ClickEvent& evt);		
protected:
	Callback<GUIMainSwipe_View, const Container&, const ClickEvent&> containerClickedCallback;
	uint8_t		CurrSubPage;

	bool SwipeContainerPage1_Pressed_status;
	int SwipeContainerPage1_Pressed_timeout;
	bool SwipeContainerPage2_Pressed_status;
	int SwipeContainerPage2_Pressed_timeout;
};

 

//In the .cpp file

GUIMainSwipe_View::GUIMainSwipe_View():
containerClickedCallback(this, &GUIMainSwipe_View::containerClickHandler)
{
 //Set curr sub page
 CurrSubPage = SwipeContainer.getSelectedPage();
}

void GUIMainSwipe_View::setupScreen()
{
 GUIMainSwipe_ViewBase::setupScreen();
 //User init code
 SwipeContainerPage1.setClickAction(containerClickedCallback);	
 SwipeContainerPage2.setClickAction(containerClickedCallback);
 ...
}

void GUIMainSwipe_View::containerClickHandler(const Container& c, const ClickEvent& evt)
{
	if (&c == &SwipeContainerPage1)
	{
		if (evt.getType() == ClickEvent::PRESSED)
		{	
			SwipeContainerPage1_Pressed_status = true;
		}
		else if (evt.getType() == ClickEvent::RELEASED)
		{
			SwipeContainerPage1_Pressed_status = false;
			SwipeContainerPage1_Pressed_timeout = 0;
		}
	}
	else if (&c == &SwipeContainerPage2)
	{
		if (evt.getType() == ClickEvent::PRESSED)
		{	
			SwipeContainerPage2_Pressed_status = true;
		}
		else if (evt.getType() == ClickEvent::RELEASED)
		{
			SwipeContainerPage2_Pressed_status = false;
			SwipeContainerPage2_Pressed_timeout = 0;
		}		
	}
}

void GUIMainSwipe_View::handleTickEvent()
{
	//Evaluate long press for page change
	if (SwipeContainerPage1_Pressed_status == true)
	{
		SwipeContainerPage1_Pressed_timeout++;
		if (SwipeContainerPage1_Pressed_timeout == GUIMAINSWIPE_BUTTON_LONG_PRESS_TIMEOUT)
		{
			goTo_GUITemperatureSet_Action();
			SwipeContainerPage1_Pressed_status = false;
		}
	}	
	if (SwipeContainerPage2_Pressed_status == true)
	{
		SwipeContainerPage2_Pressed_timeout++;
		if (SwipeContainerPage2_Pressed_timeout == GUIMAINSWIPE_BUTTON_LONG_PRESS_TIMEOUT)
		{
			goTo_GUITemperatureSet_Action();
			SwipeContainerPage2_Pressed_status = false;
		}
	}		

}

Any hint will be appreciated, thank you!

This topic has been closed for replies.

3 replies

ST Employee
Jul 22, 2025 8:20 AM UTC

Hello @MCA_Dev ,

Could you give more details. What does the goTo_GUITemperatureSet_Action() ?

BR,

 

Louis BOUDOST Software Engineer | TouchGFX
MCA_DevAuthor
Associate II
Jul 22, 2025 12:29 PM UTC

Thank you for your reply @LouisB.

The goTo_GUITemperatureSet_Action() is an action I setup from the designer to command a screen change.

void GUIMainSwipe_ViewBase::goTo_GUITemperatureSet_Action()
{
 //goTo_GUITemperatureSet_Interaction
 //When goTo_GUITemperatureSet_Action is called change screen to GUITemperatureSet_
 //Go to GUITemperatureSet_ with no screen transition
 application().gotoGUITemperatureSet_ScreenNoTransition();
}

Probably I've should've asked this question before:

is it possible to have both the swipe feature (setup from the designer, it contain two pages: SwipeContainerPage1 and SwipeContainerPage2) and setup afterwards the clickListener (in the user code) for SwipeContainerPage1 and SwipeContainerPage2 to trigger a long pressure on those containers? Or should I setup the Mixin ClickListener to the objects inside the container to make it work (for example Temp2_textArea_Page2 and Temp1_textArea_Page1) ?

MCA_Dev_0-1753186752899.png

I'm still quite new to this libraries and specifically C++, hopefully you can give me some help to make it through...

Thank you!

Best regards,

M.

MCA_DevAuthor
Associate II
Oct 10, 2025 4:12 PM UTC

I've put on hold this project for a couple of months and here I am to face this problem again...

Can anyone give me some advice on this topic?

Is it possible to insert a button inside a swipe container and can discern both the widget swipe and the individual button events?

Thank you.

Best regards,

M.