Skip to main content
unsigned_char_array
Lead III
Dec 20, 2024 1:33 PM UTC
Solved

SVG vertical gradient rendered horizonally in landscape mode

Attached SVG image with vertical gradient renders correctly in TouchGFX Designer 4.24.1, but not in the simulator.
In simulator the gradient is horizontal in landscape mode and vertical in portrait mode.

Edit. SVG attachments are banned, but renaming it to TXT is banned too so my attachment wasn't attached.

"The attachment's gradient.svg.txt content type (text/plain) does not match its file extension and has been removed."

So I've attached it as source code:

<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<!DOCTYPE svg PUBLIC "-//W3C//DTD SVG 1.1//EN" "http://www.w3.org/Graphics/SVG/1.1/DTD/svg11.dtd">
<svg width="400" height="100" xmlns="http://www.w3.org/2000/svg" xmlns:xlink="http://www.w3.org/1999/xlink">
 <defs>
 <linearGradient id="grad1" x1="0%" y1="0%" x2="0%" y2="100%">
 <stop offset="0%" stop-color="yellow" />
 <stop offset="50%" stop-color="green" />
 <stop offset="100%" stop-color="red" />
 </linearGradient>
 </defs>
 <rect width="200" height="100" x="10" y="10" fill="url(#grad1)"/>
</svg>

 

 

This topic has been closed for replies.
GaetanGodart
GaetanGodartBest answer
ST Employee
Mar 5, 2025 10:43 AM UTC

Hello @unsigned_char_array ,

 

TouchGFX 4.25.0 fixes the issue.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)

4 replies

GaetanGodart
ST Employee
Dec 27, 2024 12:38 PM UTC

Hello @unsigned_char_array ,

 

We are currently working on a similar issue  with SVG which might be related to your or be the same issue.
I will keep you updated once we fix it.

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
Jan 21, 2025 11:07 AM UTC

Hello @unsigned_char_array ,

 

Just to keep you updated, we have spotted some bugs with SVG and are fixing them.
Your issue should be part of them, I don't know exactly when it will be fixed but it will happen! :)

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
GaetanGodartBest answer
ST Employee
Mar 5, 2025 10:43 AM UTC

Hello @unsigned_char_array ,

 

TouchGFX 4.25.0 fixes the issue.

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
unsigned_char_array
Lead III
Mar 5, 2025 11:41 AM UTC

@GaetanGodart wrote:

TouchGFX 4.25.0 fixes the issue.


Confirmed. Tested with a devboard and simulator. Both landscape and portrait render properly.

"Kudo posts if you have the same problem and kudo replies if the solution works.Click ""Accept as Solution"" if a reply solved your problem. If no solution was posted please answer with your own."