Skip to main content
ykn
Associate III
Oct 9, 2019 10:45 AM UTC
Question

suggest me stm32 evaluation board having some pre example on touch screen display.

..

This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Oct 9, 2019 10:53 AM UTC

STM32H745I-DISCO​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
ykn
yknAuthor
Associate III
Oct 11, 2019 6:15 AM UTC

thank you..

this board used internal LCD-TFT cotroller.

suppose i want to use external graphics controller like SSD1963, because it has inbuilt 1215Kbytes of SRAM. so can you tell which would be cost effective, display with controller or display with without controller.

Tesla DeLorean
Guru
Oct 11, 2019 10:06 AM UTC

Perhaps look at boards from WaveShare, some of the minimal designs, with pin breakout, would allow you to wire a display​ to the external FMC bus.

​

Seem to recall GHI having a few screen options and those using controller chips.

​

Suspect you'll need to dig a bit to find boards that address your specific needs and budgetary​ goals.

​

The better model looks to be an STM32 with external SDRAM and DSI connectivity to a display. See F769I and H747I DISCO boards.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
Oct 11, 2019 11:10 AM UTC

Maybe the key question here is not "which board..." but "does such board come with example software allowing to compare...".

ST is probably not really interested in producing such, as they want to sell thechips with LTDC (read more expensive). For example, the display used on the 'F429 Disco has a QVGA display with controller which can operate either with external and internal controller, but AFAIK there's no example code using the internal-controller mode (and the board's design is not optimal to showcase that mode either).

JW

ykn
yknAuthor
Associate III
Oct 11, 2019 11:31 AM UTC

mikroe also providing the board TFT display and they are not using internal LTDC ,

they are using ssd1963 graphics controller(https://www.mikroe.com/mikromedia-7-stm32f7).

is that any benefit to use external controller. i hardly know about this TFT display with touch screen.

waclawek.jan
Super User
Oct 11, 2019 12:50 PM UTC

Looks good at the first glance.

The internal controller takes up memory bandwidth; beyond a certain size x color depth it's simply unfeasible. See AN4861.

The external controller costs money.

There may be more nuanced differences than this, but these are roughly the main game changers.

JW