Skip to main content
Sgowd.1
Associate III
June 13, 2024
Question

Storing the Images in Jpeg format for displaying GIFs in STM32U5 controller

  • June 13, 2024
  • 2 replies
  • 1496 views
Spoiler

 Storing the Images in Jpeg or png format for displaying GIFs in STM32U5 controller

Hello,

 I want to display some GIFs on my STM32U5 board. Images are stored in their raw format which is bit large in size, so is it possible to store the images in JPEG format itself, so that it consuems very less format compared to storing in raw format. I have 4-5 different GIFs to be played, and the image size of those imaqes will be way too much if it is stored in its raw format. 

Is there also any possible way where I can store the images in some compressed form?

Note: I am using STm32U5A9NJ controller which has a Hardware accelerated JPEG codec in it.

 

This topic has been closed for replies.

2 replies

GaetanGodart
ST Employee
June 24, 2024

Hello @Sgowd.1 ,

 

You only talk about storage but what about displaying your GIF?

 

First, regarding storing.
GIF uses a color palette of a maximum of 256 colors and apply LZW compression algorithm to the images. Therefore, the "raw" format of a GIF is greatly compressed already.
TouchGFX support L8 color format (the 256 color palette) as well as LZW to compress images.
So you could achieve the same result by storing each of the frames of your gifs and compressing them inside TouchGFX Designer.
JPEG will probably take more space than L8 + LZW.

"Is there also any possible way where I can store the images in some compressed form?"
I am having trouble understanding what format you currently have. Is it GIF, is it raw picture format?
If you actually have a GIF, it is already compressed.

 

Then, regarding displaying.

I see 4 options for you.

1) Displaying a video
Save your GIF as a video and display it using the video widget.

2) Displaying frame by frame by adding all images to TouchGFX Designer
For each one of your frames, add an image widget in Designer and simply display the one you need.

3) Display frame by frame by using a single bitmap
Add a single image widget to TouchGFX Designer and modify the content of the bitmap as you need to update your GIF.

4) Use an animated image widget
We have a widget called animated image which taxes n images name Whatever-1 to whatever-n. The widget will display each images one after the other based on the number at the end of the name and you can choose the speed at which the images changes.
I think this would be the easiest option for you.

Either way, if you use one of the options using images, you can compress those images to save space.

 

If this comment answers your question, I invite you to select it as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)
GaetanGodart
ST Employee
September 2, 2024

Hello @Sgowd.1 ,

 

Have you been able to solve your problem?
If so, I invite you to select the most helpful comment as "best answer".

 

Regards,

Gaetan GodartSoftware engineer at ST (TouchGFX)