Skip to main content
Associate III
Jun 13, 2025 4:59 AM UTC
Question

STMH7S7 CUBEIDE,Post Generate Target failed。

I made a test project for h7s7 using cubeIDE,the structure generated is below:

微信图片_20250613124958.png

Then I opened touchgfx designer and import a blank UI, when I tried to build the project, a error came out:

Generate Code
Generate
Wrote generated/gui_generated/include/gui_generated/screen1_screen/Screen1ViewBase.hpp
Wrote generated/gui_generated/src/screen1_screen/Screen1ViewBase.cpp
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
Unable to locate D:/STM32CubeIDE/workspace_1.7.0/7s7Test/.cproject
Failed
Failed

 

The .cproject is actually located in D:/STM32CubeIDE/workspace_1.7.0/7s7Test/Appli/.cproject

but touchgfx designer goes to  wrong folder.

Anyone who can help?

This topic has been closed for replies.

5 replies

ST Employee
Jun 18, 2025 1:44 PM UTC

Hello @amb ,

How did you created your project ,you made it from CUBEMX ?

BR,

Louis BOUDOST Software Engineer | TouchGFX
ambAuthor
Associate III
Jun 19, 2025 6:47 AM UTC

hello @LouisB 

I use CubeIDE v1.15.

I made it work by copy .cproject file to  D:/STM32CubeIDE/workspace_1.7.0/7s7Test/,

but  not a elegant solution.

ST Employee
Jun 19, 2025 8:51 AM UTC

Hello @amb,

Ok, but when you created the project it was from CubeMX or in TouchGFX designer ?

 

BR,

Louis BOUDOST Software Engineer | TouchGFX
ambAuthor
Associate III
Jun 23, 2025 12:38 AM UTC

I created the project in CubeIDE.

ST Employee
Jun 26, 2025 7:30 AM UTC

Hello @amb,

Since you create your project in CubeIDE and if you plan to Build on target from CubeIDE, this will not cause issue as the files are generated. The post generate is if you want to either run build simulator or on target from the designer.

BR,

Louis BOUDOST Software Engineer | TouchGFX