Skip to main content
Associate II
January 7, 2026
Question

STM32N657 TouchGFX RAM/ROM Overflow.

  • January 7, 2026
  • 3 replies
  • 505 views

Dear ST Community Team,

We are currently working on a project using the STM32N657X0H3Q1 microcontroller and developing the GUI application with TouchGFX.

While configuring and generating the TouchGFX project, we are encountering RAM and ROM overflow errors during compilation/linking. The internal SRAM and Flash available on the STM32N657 device are not sufficient to accommodate the TouchGFX framework, graphics assets, and application code.

As an alternative solution, our hardware design includes the following external memories:

  • External RAM: S80KS5123GABHB020

  • External Flash (Octal SPI NOR): S28HS512TGABHM0100

We would like guidance from the community on the following points:

  1. How to properly configure external RAM in STM32CubeMX / TouchGFX so that:

    • Framebuffers

    • TouchGFX heap

    • Graphics buffers are placed in external RAM instead of internal SRAM.

  2. How to configure external Flash to store:

    • TouchGFX assets (images, fonts, videos)

    • Read-only GUI resource to reduce internal Flash (ROM) usage.

  3. Any recommended linker script modifications or memory mapping examples specific to STM32N657 for placing code/data in external memories.

  4. If there are any ST reference projects, application notes, or example repositories for STM32N6 series demonstrating TouchGFX with external RAM and external Octal SPI Flash.

We would appreciate any guidance, example configurations, or best practices to resolve the RAM and ROM overflow issues using external memory.

Thank you for your support.

Best regards,

Siddu Marka.

3 replies

ST Technical Moderator
January 8, 2026

Hello @siddum.

I would recommend you to have a look at the STM32N6570-DK TBSs available in TouchGFX Designer for reference.

JohanAstrup_0-1767877353034.png

The TBSs are configured to use O-SPI flash for the TouchGFX assets. By default, the framebuffers are located in internal SRAM in the TBSs. However, it is easy to change this to PSRAM in the linker script since the PSRAM is already configured.

Best regards,
Johan

ST Technical Moderator
January 23, 2026

Hello @siddum.

Have you been able to make any progress?

Best regards,
Johan

siddumAuthor
Associate II
January 28, 2026

Hello JohanAstrup,

We are using the STM32N657X0H3Q1 microcontroller with the XSPI1 interface and have connected two external memory devices, each with an 8-bit data bus.

As described in the STM32N6 reference manual (XSPI dual-octal configuration), the two 8-bit memories are connected in parallel and together form a 16-bit wide external memory interface, sharing a single NCS signal.

In STM32CubeMX, what we have configured the XSPI peripheral as attached below.

And XSPI clock we set as 140mhz.

Could you please confirm whether this STM32CubeMX configuration is correct? If there are any additional settings or recommended , kindly let us know.

Thank you for your support.

Best regards,
siddu marka.