Skip to main content
KNguy.5
Visitor II
May 2, 2021
Question

STM32L4R5AIIx, DCMI and MT9M114 camera chip. DMA does not receive request that there is data in the DCMI data buffer.

I have been working for about 4 weeks on a project which has the STM32L4R5AIIx processor

and is using the camera MT9M114 from ON Semiconductor.

The project uses the following command to take a snap shot.

"HYPERRAM_BASE_ADDRESS" is the starting address of the HYPER-RAM memory.

HAL_DCMI_Start_DMA(&hdcmi, DCMI_MODE_SNAPSHOT, (uint32_t)HYPERRAM_BASE_ADDRESS, DATA_SIZE_WORDS)

When I looked on the scope (I checked the Line Valid line and the Frame Valid line),

I could see that data was coming out of the camera chip.

But in the DCMI Frame Event callback, there was no data in the Hyper-RAM memory.

I know that the Hyper-RAM memory is woeking because I already verified it.

I checked further and found that even though data was coming out of the camera chip,

the DMA never received a request that there was data in the DCMI buffer.

I did this by checking the value of the DMA register "DMA_CNDTRx" in the

DCMI Frame Event callback. The value of this register was not incremented to "0"

Does anyone know why the DMA does not receive a request that there was data in the DCMI buffer?

At the startup of the project I was able to configure the camera successfully through I2C.

Here is the initialization of the DCMI:

// Initialize the DCMI interface

hdcmi.Instance = DCMI;

hdcmi.Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;

hdcmi.Init.PCKPolarity = DCMI_PCKPOLARITY_RISING;

hdcmi.Init.VSPolarity = DCMI_VSPOLARITY_HIGH;

hdcmi.Init.HSPolarity = DCMI_HSPOLARITY_HIGH;

hdcmi.Init.CaptureRate = DCMI_CR_ALL_FRAME;

hdcmi.Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;

hdcmi.Init.JPEGMode = DCMI_JPEG_DISABLE;

hdcmi.Init.ByteSelectMode = DCMI_BSM_ALL;

hdcmi.Init.ByteSelectStart = DCMI_OEBS_ODD;

hdcmi.Init.LineSelectMode = DCMI_LSM_ALL;

hdcmi.Init.LineSelectStart = DCMI_OELS_ODD;

// Initialize the DMA Channel

hdma_dcmi.Instance = DMA1_Channel1;

hdma_dcmi.Init.Request = DMA_REQUEST_DCMI;

hdma_dcmi.Init.Direction = DMA_PERIPH_TO_MEMORY;

hdma_dcmi.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_dcmi.Init.MemInc = DMA_MINC_ENABLE;

hdma_dcmi.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;

hdma_dcmi.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;

hdma_dcmi.Init.Mode = DMA_NORMAL;

hdma_dcmi.Init.Priority = DMA_PRIORITY_HIGH;

if (HAL_DMA_Init(&hdma_dcmi) != HAL_OK)

{

  Error_Handler();

}

__HAL_LINKDMA(hdcmi,DMA_Handle,hdma_dcmi);

HAL_NVIC_SetPriority(DCMI_IRQn, 5, 0);

HAL_NVIC_EnableIRQ(DCMI_IRQn);

/* DMA1_Channel1_IRQn interrupt configuration */

HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 5, 0);

HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);

/* DMAMUX1_OVR_IRQn interrupt configuration */

HAL_NVIC_SetPriority(DMAMUX1_OVR_IRQn, 5, 0);

HAL_NVIC_EnableIRQ(DMAMUX1_OVR_IRQn);

This topic has been closed for replies.