Skip to main content
bob jones
Associate
Apr 7, 2018 6:19 AM UTC
Question

STM32L100C-DISCO odd LCD issue

Posted on April 07, 2018 at 08:19

Hello, So I am using a STM32L100C-DISCO to display some numbers on an LCD display, I am using the LSI as the clock source. My program works fine for a couple of hours, but if I de-power then power-on the board, the LCD booster circuit does not turn on. I thought this might be a board malfunction because of me blowing it up, but everything else works. I then bought another of the exact same board and tried it. Does the exact same thing as the first board. But now if I leave the first board unplugged for a couple of hours the LCD booster circuit on the that powers on, and my program works fine. I tried this with the second board but with it still plugged into the LCD but with no power, and the booster circuit wont start up. I have no explanation for this. I am using AC6 with the latest firmware.

thanks

#lcd #stm32l1

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This topic has been closed for replies.

10 replies

waclawek.jan
Super User
Apr 7, 2018 10:21 PM UTC
Posted on April 08, 2018 at 00:21

What LCD? What booster circuit? Why do you think this is STM32-related?

JW

T J
Senior III
Apr 8, 2018 12:59 AM UTC
Posted on April 08, 2018 at 00:59

sounds like the LCD backlight,

do you have a dimmer function ?

bob jones
bob jonesAuthor
Associate
Apr 8, 2018 7:01 AM UTC
Posted on April 08, 2018 at 07:01

The LCD booster circuit is meant to control the contrast of the LCD, it also acts as the power supply for the LCD. But I dont have a function for this, the contrast is automatically set in the CubeMx setup