Skip to main content
MLook.1
Associate II
September 7, 2021
Question

STM32H7B3I DK/TouchGFX Designer 4.17 Cannot create new projects

Since upgrading from 4.15 I've not been able to create new blank projects or any of the examples when selecting by board. The error message is: "Combination of STM32H7B3I & Blank UI failed" for the blank example the version is v 3.0.7 which appears to be the most recent.

This topic has been closed for replies.

10 replies

Romain DIELEMAN
ST Employee
September 7, 2021

Hi,

This is strange. Could you try to go to the %appdata% folder and then to the /Roaming/TouchGFX-4.17.0 and share the TouchGFX logfile ? Then delete what is inside the folder, open TouchGFX Designer again and try to create a project with the STM32H7B3dk

/Romain

MLook.1
MLook.1Author
Associate II
September 7, 2021

Here is the log before a clear out after attempting to create a blank project

Romain DIELEMAN
ST Employee
September 7, 2021

Thank you for the log files. In the mean time as a workaround, add the shared tpa file to the C:\TouchGFX\4.17.0\app\packages folder, open Designer and try to create a project again.

/Romain

EDIT: i sent the v3.0.6 instead of 3.0.7, give it a try anyway