Skip to main content
Karan 123
Senior
May 17, 2020
Question

STM32H7B3 GFX Resolution Supports and Frame Buffer Calculation:

Hello,

STM32H7B3xI is coming with approx . 1.4MB Internal RAM .

What max TFT resolution it will supports with Internal Frame Buffer (Single Buffer)

only with single MCU?

Frame Buffer = Number of Pixels x ( Color Depth in Bits / 8 ) 

Frame Buffer = 800 x 480 x ( 16/ 8 ) 

Frame Buffer = 768000 Bytes

Frame Buffer = 750 KBytes

--

Karan

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
May 17, 2020

Theoretically, you can do the calculations, but you also need to consider the complexity of the application vs the "Max Resolution".

Karan 123
Karan 123Author
Senior
May 17, 2020

Thanks..

​

​​Ok..

​

My Application has Scroll Lists, Text Areas, Buttons with Multiple Screens.. No Video No Heavy Graphics and No Animations Required. Just for Industrial HMIs.

​

1) How to Distinguish RAM from

Fram Buffer and Rest of RAM for application part.

​

​

2)​ Is there any Eval/Development that have 7 inch TFT 800 x 480 ResolutionResolution with RGB Interface?

​

​

--

Karan​

​

​