Skip to main content
DFerl.1
Visitor II
May 28, 2020
Question

STM32H7B3 Discovery Kit and TouchGFX Designer 4.13.0 Generate Code/Run Target/Run Simulator very very slow

Using TouchGFX Designer 4.13.0 with my Discovery Kit STM32H7B3 I have problem during Generate Code - Run Target and Run Simulator: it takes 5 to 10 minutes to generate Assets or starting simulator.

I have a Win10 Pro 64 Bit, 32GB Ram, Intel i7 vPro 8th Gen, SSD HDD.

As I saw in other post, I also disabled Avira Antivirus but without success.

Could you please help me?

Thanks

This topic has been closed for replies.

4 replies

Alexandre RENOUX
Visitor II
August 17, 2020

Hello,

Did you solve your problem ?

/Alexandre

VSilv.11
Visitor II
August 27, 2020

I have the same issue! Really,really slow !

Alexandre RENOUX
Visitor II
August 27, 2020

Hello,

Could you try installing TouchGFX 4.14 and see if it behaves the same ?

Is it the same if you choose another Application Template ?

/Alexandre

Martin KJELDSEN
Principal III
August 28, 2020

Does the same thing happen if you compile using the TouchGFX Environment?

make -f simulator/gcc/Makefile