Skip to main content
Visitor II
Jul 9, 2024 1:27 AM UTC
Question

stm32h7b0 has UNALIGNED hardfault problem when using lvgl9.1

Use sthm32h7b0 to push 800*480 TFT screen, using internal ram,using RGB565 color space. Run the test function lv_demo_widgets(), it can work normally under lvgl8.2. fter lvgl was upgraded from version 8.2 to version 9.1, after modifying the corresponding driver file, run the lv_theme_default_init function under the lv_demo_widgets function, and hardfault occurs. 

```
msh />psr: 0x01000000
r00: 0x0000000f
r01: 0x08084d7f
r02: 0x00000000
r03: 0x08084d70
r04: 0x240c21a4
r05: 0x240c21a0
r06: 0x240c219c
r07: 0xdeadbeef
r08: 0xdeadbeef
r09: 0xdeadbeef
r10: 0xdeadbeef
r11: 0xdeadbeef
r12: 0x00000000
 lr: 0x08029019
 pc: 0x08043636
hard fault on thread: LVGL
rt_thread_ thread   pri  status      sp     stack size max used left tick  error
---------- -------- ---  ------- ---------- ----------  ------  ---------- ---
0x240cc338 wav_p     15  suspend 0x000000c4 0x00000800    09%   0x0000000a EINTRPT
0x240cba94 k20s imp  16  suspend 0x000000e0 0x00000800    10%   0x0000000a EINTRPT
0x240cb5f0 k20s tx   15  suspend 0x000000a4 0x00000400    16%   0x0000000a EINTRPT
0x240cb14c k20s rx   15  suspend 0x000000b8 0x00000400    17%   0x0000000a EINTRPT
0x240ca4ec k20s imp  16  suspend 0x000000e0 0x00000800    10%   0x0000000a EINTRPT
0x240ca048 k20s tx   15  suspend 0x000000a4 0x00000400    16%   0x0000000a EINTRPT
0x240c9ba4 k20s rx   15  suspend 0x000000b8 0x00000400    17%   0x0000000a EINTRPT
0x240c7744 LVGL      25  running 0x00000048 0x00002000    01%   0x0000000a OK     
0x240c658c tshell    20  suspend 0x000000b8 0x00001000    04%   0x0000000a EINTRPT
0x240bff28 LVGL      25  ready   0x00000048 0x00002000    00%   0x0000000a OK     
0x240c3794 audio     14  suspend 0x000000a8 0x00000400    16%   0x00000001 EINTRPT
0x240024b0 usbd       8  suspend 0x000000c0 0x00001000    04%   0x00000014 EINTRPT
0x240037ac tidle0    31  ready   0x0000004c 0x00000100    29%   0x0000000e OK     
0x240c2470 main      10  suspend 0x00000124 0x00000800    41%   0x00000006 EINTRPT
usage fault:
SCB_CFSR_UFSR:0x100 UNALIGNED
```
Specifically locate the lv_palette_main function, and a non-alignment error occurs when returning.The location where the hardfault occurs is as follows:
 
1.jpg
 
```
typedef struct {
    uint8_t blue;
    uint8_t green;
    uint8_t red;
} lv_color_t;
```
lv_color_t is changed to 3 bytes. return colors[p]; When the statement runs, a hardfault occurs when half-word is loaded from address 0x8084d7F to register R2.
The value of SCB->CCR is 0x70200
 
```
  MPU_InitStruct.Enable = MPU_REGION_ENABLE;
  MPU_InitStruct.BaseAddress = FLASH_BANK1_BASE;
  MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
  // MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
  MPU_InitStruct.AccessPermission = MPU_REGION_PRIV_RW_URO;
  MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
  MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
  MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
  MPU_InitStruct.Number = MPU_REGION_NUMBER3;
  MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
  MPU_InitStruct.SubRegionDisable = 0x00;
  MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
```

I would like to ask everyone, can stm32h7 not access the internal Flash in an unaligned manner? Is there any way to solve this problem?
This topic has been closed for replies.

2 replies

Explorer
May 29, 2025 4:48 AM UTC

Was there any solution for this? I'm getting a hardfault at the same point

GGODA
Associate II
May 30, 2025 9:30 AM UTC

Hello @tmit ,

 

It is probably bets for you to create a new thread and to explain in detail wat hardware you use, what software you use and how to reproduce the error.

 

Regards,