Skip to main content
Caan
Associate III
Nov 28, 2025 1:55 PM UTC
Question

STM32H750B-DK: Can't run TouchGFX with Dual QSPI (2NA17 RW213) and SDRAM IS42S32400J

I have designed a board with STM32H750B-DK With exact same pin configuration with QSPI amd SDRAM connected exactly to the reference board.
QSPI is running properly by viewing using STM CUBE Programmer (External loader selected)
But when I am using touchg GFX sample code it gives Hardfault error I believe that SDRAM is failing. (I have removed the touch screen routine to check the flow of code)

2 replies

mƎALLEm
ST Technical Moderator
Nov 28, 2025 3:00 PM UTC

Hello,

Before adding TouchGFX, try to test SDRAM by doing write/read accesses, at least to validate your SDRAM hardware.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Caan
CaanAuthor
Associate III
Nov 28, 2025 4:38 PM UTC

The given example of cube h7 is giving errors and it is not working with orignal stm32h750b-dk also