Associate III
Apr 6, 2025 7:27 PM UTC
Solved
STM32H743 LTDC Problem
- 5 replies
- 1101 views
Hey,
I have a confusing error, i have a Riverdi 7" TFT Panel (https://download.riverdi.com/RVT70HSTNWC00-B/DS_RVT70HSTNWC00-B_Rev.1.2.pdf)
Actually my LTDC Init is this:
static void MX_LTDC_Init(void)
{
/* USER CODE BEGIN LTDC_Init 0 */
/* USER CODE END LTDC_Init 0 */
LTDC_LayerCfgTypeDef pLayerCfg = {0};
/* USER CODE BEGIN LTDC_Init 1 */
/* USER CODE END LTDC_Init 1 */
hltdc.Instance = LTDC;
hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
hltdc.Init.HorizontalSync = 0;
hltdc.Init.VerticalSync = 0;
hltdc.Init.AccumulatedHBP = 160;
hltdc.Init.AccumulatedVBP = 23;
hltdc.Init.AccumulatedActiveW = 1184;
hltdc.Init.AccumulatedActiveH = 623;
hltdc.Init.TotalWidth = 1344;
hltdc.Init.TotalHeigh = 635;
hltdc.Init.Backcolor.Blue = 0;
hltdc.Init.Backcolor.Green = 0;
hltdc.Init.Backcolor.Red = 0;
if (HAL_LTDC_Init(&hltdc) != HAL_OK)
{
Error_Handler();
}
pLayerCfg.WindowX0 = 0;
pLayerCfg.WindowX1 = 1024;
pLayerCfg.WindowY0 = 0;
pLayerCfg.WindowY1 = 600;
pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
pLayerCfg.Alpha = 255;
pLayerCfg.Alpha0 = 255;
pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_CA;
pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_CA;
pLayerCfg.FBStartAdress = 0xC0000000;
pLayerCfg.ImageWidth = 1024;
pLayerCfg.ImageHeight = 600;
pLayerCfg.Backcolor.Blue = 255;
pLayerCfg.Backcolor.Green = 0;
pLayerCfg.Backcolor.Red = 0;
if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN LTDC_Init 2 */
/* USER CODE END LTDC_Init 2 */
}the Layer0 background is set to blue, if my WindowsX1 = 1024, my background shows no blue screen, but only gray..
if i decrease WindowX1 to 500, then my screen is half blue, if i change WindowsX1 to 0 then my Screen are complete blue..
whats wrong? my LCD is in 18-Bit mode (RGB666) and V/HSync and the DCLK of the display is 50 MHZ, Pixel Format is set to RGB888.
my external sdram works fine, here is the test result:
-------------------- SDRAM 16 bit access -------------------
Write 16-bit data , size: 32 MB, elapsed time: 825 ms, write speed: 38.79 MB/s
Read 16-bit data, size: 32 MB, elapsed time: 3161 ms, read speed: 10.12 MB/s
-------------------- 16 Bit data validation -------------------
SDRAM 16-bit data validation pass!