Skip to main content
GChen.5
Associate II
Mar 20, 2022 3:27 PM UTC
Solved

STM32H735G-DK's DMA2D Start Address Drifts

I'm using CubeMX to generate the start file rather than the BSP example. When I tried to set the DMA2D, I found that the start address will be shifted by 0xC.

...
// setup octospi2 for hyperram, dma2d and ltdc above
uint32_t col;
uint32_t startAdd = 0x70000000; // try to write the hyperram at this address
// use dma2d to write 0xFF224433 to the startAdd
HAL_DMA2D_Start(&hdma2d, 0xFF224433, (uint32_t)startAdd, 6, 1);
 
// try to verify the data in hyperram
for (int i = 0; i < 272; i++) {
 for (int j = 0; j < 480; j++) {
 uint32_t add = (startAdd + (i * 480 + j) * 4);
 col = *(uint32_t *)add;
 if (col == 0xFF224433)
 DEBUG_PRINT_USB("find color at <%d, %d> 0x%x\n", j, i, add);
 }
}
 
// the output is:
find color at <3, 0> 0x7000000C
find color at <4, 0> 0x70000010
find color at <5, 0> 0x70000014
find color at <6, 0> 0x70000018
find color at <7, 0> 0x7000001C
find color at <8, 0> 0x70000020
 
// the start address is shifted by 0xC, whatever start address x I give to the DMA2D, I always read the first value at (x+0xC), what's the problem?

This topic has been closed for replies.
GChen.5
GChen.5Best answer
Associate II
Mar 20, 2022 4:13 PM UTC

I solved the problem, when I set the S70KL1281, the latency should be set to 3 instead of 6.

S70KL1281_WriteCfgReg0(&hospi2, reg, HAL_OSPI_FIXED_LATENCY, OPTIMAL_FIXED_INITIAL_LATENCY); // the OPTIMAL_FIXED_INITIAL_LATENCY=3

2 replies

GChen.5
GChen.5AuthorBest answer
Associate II
Mar 20, 2022 4:13 PM UTC

I solved the problem, when I set the S70KL1281, the latency should be set to 3 instead of 6.

S70KL1281_WriteCfgReg0(&hospi2, reg, HAL_OSPI_FIXED_LATENCY, OPTIMAL_FIXED_INITIAL_LATENCY); // the OPTIMAL_FIXED_INITIAL_LATENCY=3

MM..1
Super User
Mar 20, 2022 4:32 PM UTC

Your FOR check code is quicker as DMA ... try add

HAL_DMA2D_PollForTransfer(&hDma2dHandler, 10);