Skip to main content
Woula
Associate II
Dec 30, 2022 1:55 AM UTC
Question

STM32F7508-DK : Blank screen after flashing TouchGFX GUI

Hi,

I am trying to flash a single screen Touch GFX application on my STM32F7508-DK board but I got a blank screen.

Did anyone face that problem before ? What could be the solution ?

My actual configuration:

TouchGFX Designer 4.21.0

Thanks in advance!

This topic has been closed for replies.

3 replies

Karl Yamashita
Super User
Dec 30, 2022 2:38 AM UTC

Do you mean the STM32H750B-DK? Did you press the black reset button? I'm working on this board this very minute. Unlike other TouchGFX projects, this one does not start after being programmed from STM32CubeIDE until you reset it.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Woula
WoulaAuthor
Associate II
Dec 30, 2022 4:03 AM UTC

No. I think they are different.

I did press the reset button many times but nothing had changed.

Even the examples are not displayed after being flashed. The screen remains blank.

Karl Yamashita
Super User
Dec 30, 2022 10:21 AM UTC

Have you've checked to see if the External Loaders section has a memory device selected?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source